Part Number: TPS22968-Q1 Hi team,
I would like to estimate the min and max value of Tr for given CT value.
I set CT so that the tr get 5ms.
Should I consider CT(uF) value variation over temperature only?
Is there temperature variation inside the device…
Part Number: TPS22968-Q1 Hello,
can you please provide the abs maximum rating for the CTx Pins. How much voltage can the pins withstand.
What is the minimum needed voltage when I want to bias the charge pump externally?
For example I have 3.3Vin, can…
Part Number: TPS22968 Other Parts Discussed in Thread: TPS22950 , TPS27S100 , TPS2660 Hi team,
My customer is asking load switch solution and below is main specification they need.
1. output current>2A
2. need external Ilim pin to program output current…
Part Number: TPS22968-Q1 Hi
I'm experiencing something I didn't expect using this switch. I'm using it in reverse current protection configuration.
My EN signal is 3.3V and my bias voltage is 4.5V.
If I close the switch, but I don't have…
Part Number: TPS22968 Other Parts Discussed in Thread: TPS22917 , TPS22916 , TPS22953 , TPS2115A Hi TI-Team,
will the TPS22968 work for connecting two batteries individually to a BQ24210DQCT charger IC? We will charge only one battery at a time and I don…
Part Number: TPS22968-Q1 Other Parts Discussed in Thread: TPS22968 , TPS22966 , TPS25940-Q1 , TPS22966-Q1 , Dear expert,
Happy new year!
I see two similar laod switch TPS22966 and TPS22968, I first choose 66 for lower Rdson. However, I noticed that although…
Part Number: TPS22968 IC Part no.:
TPS22968DPUR
Conditions:
I/P power rails: VCC_5V & VCC_1V8
O/P power rails: VAN_5V & VDD_1V8
ON1 is controlled by VDD_1V8.
ON2 is controlled by VCC_1V8.
Requirement:
Sequenced power out VDD_1V8 --(Delay ~10…
Part Number: TIDA-00663 Other Parts Discussed in Thread: TPS22968 Hello
Here is a part of the TIDA-00663 , LIDAR Pulsed Time of Flight Reference Design.I would like to know the role of TPS22968 except “digitally calibrate”,because I found that there is a…