Part Number: TPS22968-Q1 Tool/software: Hello,
Could you help determine what is the ON pins (pin 2, 4) logic voltage thresholds are with 5.0V Vbias and 3.3V Vbias.
The datasheet, section 7.3 seem to only have operating min max range and unclear…
Part Number: TPS22968-Q1 Other Parts Discussed in Thread: LM61440-Q1 Tool/software: hi TI expert, the schematic shown as below, we found that 1/4W fail rate that the bias pin of the TPS22968-Q1 burnt and open , could you help to analyze the reasons, thanks…
Part Number: TPS22968-Q1 Tool/software: Dear Team,
We are using the module TPS22968NQDMGTQ1 in our new design. Project Application : Telematics ODB Dongle Please find the schematics section attached.
Please review it and share your feedback with…
Part Number: TPS22968-Q1
Tool/software:
Table 1 (Rise Time Table) in the TPS22968-Q1 datasheet (Rev B) doesn't appear to correlate with the slew rate equation. The datasheet shows as follows:
However, if I calculate the table based on the slew…
Part Number: TPS22968-Q1 Other Parts Discussed in Thread: TPS22916 , TPS22918-Q1 , TPS22976 , TPS22810-Q1 , TPS22919-Q1 , TPS22919 , TPS22918 , TPS22990 Hi TI Team,
I want to use Load Switches in My Application. But in Most of the Switch Datasheets…
Part Number: TPS22968-Q1 Hi team,
I would like to estimate the min and max value of Tr for given CT value.
I set CT so that the tr get 5ms.
Should I consider CT(uF) value variation over temperature only?
Is there temperature variation inside the…
Part Number: TPS22968-Q1 Hello,
can you please provide the abs maximum rating for the CTx Pins. How much voltage can the pins withstand.
What is the minimum needed voltage when I want to bias the charge pump externally?
For example I have 3.3Vin…
Hi Jiang,
Thanks for reaching out on E2E and being patient as many of us are returning from holidays! Happy Holidays!
The TPS22966-Q1 is an older device, we don't generate SOA curves for other load switches including the TPS22968-Q1.
The SOA curve…
Part Number: TPS22968-Q1 Hi
I'm experiencing something I didn't expect using this switch. I'm using it in reverse current protection configuration.
My EN signal is 3.3V and my bias voltage is 4.5V.
If I close the switch, but I don't have anything…