Part Number: TPS22971
Hi, Team
I designed a power circuit for SD CARD with TPS22971 like figure.
The circuit operates as the following: step1. Enable TPS22971 and Vout rises to VIN(3.3V) step2. VIN falls from 3.3V to 1.8V. step3. VIN rises to 3…
Part Number: TPS22971 Other Parts Discussed in Thread: TPS22918-Q1 , , TPS22966-Q1 , TPS22966 Hello,
Are there any plan to release of TPS22971-Q1 ? Our customer request the power switch which has following specifications.
Vin : under 1V to 3.5V Iout…
Part Number: TPS22971 Hi
We got a question from customer about TPS22971.
They desire slew rate 25mV/μs at turn off.
How is the slew rate determined at turn off?
Thanks.
Sincerely.
Part Number: TPS22971 Dear Forum
I have a whole cascade of high side switches in my design and am somewhat stuck with the PG output of TPS22971
Now, I have the following situation VIN1/2 = 0V (i.e. the input voltage is not yet enabled), ON (PGOOD9…
Part Number: TPS22971 Hi team,
My customer has a question TPS22971-
To double check, when it says the slew rate capacitor CT is 0 pF that means the pin should be left open and floating? for Vin = 1.05V rails and a fast turn-on time?
Also …
Part Number: TPS22971 Team,
the switching characteristics in our datasheet state tON values for certain CT value test conditions. My customer is struggling to calculate these values using formula 2.
Example using
VIN = 3.6V
CT = 1000pF
Using…
Part Number: TPS22971 Hi team,
As you know , TPS22971 been use in intel VCCST rail. Intel request <=300ohm during discharge.
Our datasheet just show 3.6V and 0.65V. What's the pull down resistor at 1.05V?
Thanks
Shaq.
Part Number: TPS22971 Other Parts Discussed in Thread: TINA-TI Hello,
In below post, adding input capacitor of TPS22971 helps the voltage drops due to inrush current when trun-on. Is there any guidance how much input capacitor would be good? I think…
Part Number: TPS22971 Other Parts Discussed in Thread: TPS27081A Hello,
We are thinking to use load switch as below circuit. They are using TPS27081 but change from TPS27081 to TPS22971.
In TPS22971 datasheet, rampup waveform is smoothly(linearly…