Part Number: TPS22992 Other Parts Discussed in Thread: TPS25947 Tool/software: Hi Team,
1.We are working on a project , which is using USB Type C, sink mode, 5V,3A design. The capacitor value is greater than 200uF because of circuit limitations. In…
Part Number: TPS22992 Tool/software: To whom it may concern -
How is the charge pump used inside the device?
If the charge pump is lower than the recommended voltage range (< 1.5V), how does the circuit respond?
Thanks,
Brendan
Part Number: TPS22992 We would like to request a design review for the power section. Kindly share your review comments at the earliest possible. TPS22992SRXNR -Load switch.pdf
Part Number: TPS22992
Tool/software:
Hello,
We are doing thermal calculation for TPS22992. We required maximum allowable junction temperature of this IC, which is not given in the datasheet. I have attached the screenshot for your reference.
Part Number: TPS22992 Tool/software: Hello,
My customer is looking for load switch solution that supports the following conditions.
- VIN = 3.7V (18650 Battery)
- VOUT = 3.7V / 30A (Solutions to minimize heat generation)
If there is a TI product…
Part Number: TPS22992 Tool/software: To whom it may concern -
Per the datasheet, it states if we want to use the internal resistance for discharge of VOUT, we can short QOD to VOUT. With a 100 ohm resistance, what is the power rating on that internal…