Part Number: TPS22995H-Q1 Tool/software: Hi Team,
We are using TPS22995HQDDCRQ1 in our project, we provided 3.3V as input the switch , As indicated in datasheet when EN pin is driven high from microcontroller, power switch output is high(+3.3V), but…
Part Number: TPS22995H-Q1 Tool/software: From the datasheet, we know the maximum continuous current is 3A. What is the test condition of 3A? With calculation, 3A won't trigger thermal shutdown protection.
Part Number: TPS22995H-Q1 Tool/software: Hi team,
My customer would like to use TPS22995H-Q1 with 3.3V of the input voltage. To enable TPS22995H-Q1, my customer plans to use 1.8V logic supply, so above 1V of VIH is needed. How does TPS22995H-Q1 determine…
Part Number: TPS22995H-Q1 Tool/software: Hi Team,
For TPS22995H-Q1 operating condition.
VIN=VBIAS <0.8V, VON=3.3V condition, what VOUT status it has?
BR.
Lenny Lee.
Part Number: TPS22995H-Q1 Tool/software: Hi, looking for reflow profile or soldering profile details for TPS22995HQ1
Can you please share the concerned document.
Part Number: TPS22995H-Q1 Other Parts Discussed in Thread: TPS22999 , TPS22954 Tool/software: Team,
do we have an alternative in our portfolio (or on roadmap) that is similar to TPS22995H-Q1 but has a QOD resistor of 10 Ohms?
Best regards
Part Number: TPS22995H-Q1 Hello,
the maximum on-resistance is specified for VBIAS = 3.3 V, VIN = 3.3 V and IOUT = -200 mA with 29 mOhm for the temperature range -40..125 °C.
Please specify the maximum on-resistance for currrents up to -3 A.
Thanks…