Part Number: TPS22996 Tool/software: Under the recommended operating conditions in the datasheet it is stated that the Input voltage must be less then Vbias.
What are the consequences of having VIN > Vbias? I.e. Vbias=3.3V VIN=4V?
Part Number: TPS22996 Tool/software: On the main page for the device it is stated that the shutdown current is 0.0001uA, but the data sheet states typ. 0.1uA max. 0.5uA.
Can you pls. clarify which is correct?
Part Number: TPS22996 Can you please find out what the charge pump frequency is of this device? I did not see it (or missed it) in the datasheet.
Thank you.
Mike
Part Number: TPS22996 Tool/software: Hi,
We need TPS22996N- 2-ch, 5.5-V, 4-A, 14-mΩ on-resistance load switch with adjustable rise time (WITHOUT QUICK OUTPUT DISCHARGE feature).
How can I order the part? What is the orderable part number?
If…
Part Number: TPS22996 Other Parts Discussed in Thread: TPS22991 , TPS22995 , BQ2970 Tool/software: For a battery charger based on the BQ2562X, where a battery "pack" is inserted into the charger by the user, and the user must press a button to begin charging…
Part Number: TPS22996EVM Other Parts Discussed in Thread: TPS22996 , Tool/software: The TPS22996EVM is missing pull-down resistors on the ON1 and ON2 inputs on the TPS22996 device. Once enabled with one of the DIP switches (SW1 or SW2) the given output…
Part Number: LM7310 Other Parts Discussed in Thread: TPS22996 , Tool/software: Hi Team,
My customer is looking for 2nd source of APL3573BQBI-TRG TQFN 16P PW SWITCH, TI Cross Reference tool show LM73100, would you please suggest if any other more suitable…
Part Number: ISOW7741 Other Parts Discussed in Thread: TPS22996 Great part! I have a 5V to 5V isolation barrier working with the EN_IO pin floating (enabled). EN/FLT is pulled up to VIO with 100K. With Vdd power at 5V the current into VIO is 4mA. With…
Part Number: TPS22966-Q1 Hi,
Im an AE for the USB gruop, and I'm looking for a Vbus switch that has fault detection built in.
I need the switch be rated for 5V 4A-6A with an error detect signal.
The TPS22996-Q1 has the rating I need, but does not…
Part Number: SN74ACT244 Other Parts Discussed in Thread: SN74LVC2G07 , SN74LXC8T245 , TPL7407LA , TPS22996 , TPS22960 , TXU0104 , SN74LXC2T45 , CSD13381F4 Tool/software: Hello,
I have 8 LED and each LED can have a forward current of 25mA with forward…