Part Number: TPS23521EVM-001 Other Parts Discussed in Thread: TPS23523 , TPS23521 Sir / Madam,
We are using TPS23521EVM-001 unmodified along with a Power Supply targetted for compliance and did a surge test.
The Power Entry connector has a TVS Diode…
Thanks for reaching out. Implementing soft start mechanism by placing external C DVDT capacitor is not very easy option in LM5064. I would suggest you use TPS23521 + INA226 (for PMBus monitoring). Please see the below EVM user's guides.
TPS23523EVM…
Hi Rakesh
I Tested the TPS23521EVM-001 for below Condition.
VIN : -48V
VOUT : -48V
LOAD Current : 7A
When Q2 Gate Enable, It does not operate due to inrush current.
but When the load current is reduced to 2A, it does operate.
TPS23521EVM…