Part Number: TPS2372-4EVM-006 Tool/software: Could share the TPS2372-4EVM-006 of the Gerber and Bom list? My customer wants to build the board by themself.
BR,
Gary
Part Number: TPS2372-4EVM-006 Tool/software: Hello,
I'm building a 802.3bt PoE PSE and I want to test it. I see there is the eval board TPS2372-4EVM-006. It is possible to test my PSE with it?
I want to test:
- single and dual-signature.
- power…
Part Number: TPS2372-4EVM-006 Tool/software: Hello TI team.
Recently I found and issue with the TPS2372-4 evaluation board.
If connected to a PoE++ injector of type POE-171A-95 or POE-171A-60 (manufactuer PLANET, see image attached) I will get unexpected…
Part Number: TPS2372-4EVM-006 Other Parts Discussed in Thread: LM70880 Tool/software: Hi Team,
Test TPS2372-4 EVB, When using BULLET POE IP SWITCH for power supply testing, Test output perform power, IP SWITCH will actively protect mode, The Startup…
Part Number: TPS2372-4EVM-006 Other Parts Discussed in Thread: PMP20859 Q1:If I use the FDMQ8205A(ideal diode bridge) in the TPS2372-4EVM-006, how does the FDMQ8025A block reverse current to each other?
e.g, if the signal pair input is +57V, and the…
Part Number: TPS2372-4EVM-006 Hi,
I designed a costum board by takind an example of TPS2372-4EVM-006 and it works. I have a problem when ı set resistor values of CLSA and CLSB. I assigned CLSA pin as 63.4R and CLSB pin 90.9R for 70w power request from…
Part Number: TPS2372-4EVM-006 Can you explain how IEEE 802.3at-2009 Class 1 and 2 power levels between PSE (Pclass) and PD (Ppeak_PD) can be compatible given Table 33-7 Pclass supply limits (4W and7W) are less than Table 33-18 Ppeak_PD consumption limits…