Part Number: TPS23730EVM-093 Other Parts Discussed in Thread: UCC2897A , , PMP23253 Hello Expert,
Our customer is designing POE PD BT circuit which is configured with TPS2373-4 and UCC2897A.
In the case of FORWARD CONVERTER, I know that MAX DUTY should…
Part Number: TPS23730EVM-093 Hello,
This is a suggestion for TPS23730EVM-093's user guide: The schematics are all low-resolution raster graphics.
In the next revision of the PDF, could these please be vector-graphics instead, preferably with searchable…
Part Number: TPS23730EVM-093 Other Parts Discussed in Thread: TPS23730 HI, I am planning to purchase TPS23730EVM-093 EVM. It supports for 12V Supply Only. My Requirement is 24V. How can it be achieved with the same EVM? Or suggest for another EVM which…
Part Number: TPS23730EVM-093 Other Parts Discussed in Thread: TIDA-050045 , TPS23730 Hi Team,
We have purchased the a.m. EVM for a 20-69V input to 12V/2.5A output: we decided to adopt the design as is.
We now need to provide 5.25V/6A at the output…
Part Number: TPS23730EVM-093 The TPS23730EVM-093 output inductor L8 is drum core inductor which is very large (18.3x8.9x18.2mm , 14A)
Can you recommend smaller size inductor?
Part Number: TPS23730EVM-093 Other Parts Discussed in Thread: TPS23730 Hello team,
my customer is currently evaluating with the TPS23730EVM-093, has asked if the board can be modified to output 48V?
is there a reference design for 48V output with…
Part Number: TPS23730EVM-093 1) Page 11, section 5
- typo : should be Vadptr_on instead of Vadptr_off
- the calculation result of Rapd1+Rapd2 is incorrect: should be 69.23+3.01=72.24 and not 72.81
2) Page 11, section 6 - what is the Vapdh ?
…
Part Number: TPS23730EVM-093 Hi,
We have just brought up our first revision/proto board using this evaluation circuit for our PoE PD. We have been doing some measurements on efficiency and the results correlate pretty well with the measurements you…