Part Number: TPS2375 Other Parts Discussed in Thread: TPS23861 Good Morning,
We've got a design featuring a TPS23861 PSE controller which we're using to power another design using a TPS2375D PD Controller.
We're seeing issues where the TPS23861 is…
Part Number: TPS2375 HI
I'm currently using TPS2375, and after a successful PD negotiation, it supplies power to the DCDC converter to generate 12V.
However, when I turn off and on the DCDC converter again, it seems that TPS2375 is triggering the…
Part Number: TPS2375 Tool/software: Hi
I am using TPS2375 for PoE in a PD. Below is the related schematic:
PD class is set to Class 0.
At first I had 0E in place of 2.2uH then I was seeing below output across 100uF capacitor on the output of…
Part Number: TPS2375 Other Parts Discussed in Thread: TPS2376 , , TPS2377 HI
Is there an 802.3at TYPE 2 CLASS2 or 802.3bt capable IC that is PIN to PIN compatible with the TPS2375?
Part Number: TPS2375 Other Parts Discussed in Thread: TPS2376 , , TPS2377 HI
Is there an 802.3at TYPE 2 CLASS2 or 802.3bt capable IC that is PIN to PIN compatible with the TPS2375?
Part Number: TPS2375 Other Parts Discussed in Thread: LM5116 , LM70840 , LM70860 Tool/software: I'm looking at a replacement for and design for this part https://www.senliwell.com/product/155.html
Thoughts?
Part Number: TPS2375 Hello, I am needing to create a 13 watt PoE power source, which eventually provides a 12VDC power rail to the PCB. I attached the schematic I currently implemented (see below).
The problem with this is that I need isolation, since…
Part Number: TPS2375-1 Tool/software: Hi team,
The PG pin of the TPS2375PWR-1 is an open-drain output. If the PG output is not being used, is it OK to leave it open without inserting a pull-up resistor?
Thank you for your help.
Regards,
Taito…
Part Number: TPS2375
Has anyone tried using the TPS2375 with the Cqenpr brand of PoE switches? When I look at the scope grab on page 1 of the TPS2375 data sheet it looks like the voltage is rising in a slow and controlled manner. When I connect my device…