Part Number: TPS23751 Hi TI member,
Please help to review our schematic which uses PD function IC TPS23751, and our requirement as below, thanks.
PD Vin: +48-52V
Vout: 24V / 1A
SCH_RemoteIO_2026-07-27.pdf
Part Number: TPS23751 Tool/software: We are currently using the EVK circuit and have found that the high-speed signals on the board are being interfered with by the transformer. Are there any methods or countermeasures to resolve this issue?
Part Number: TPS23751 Other Parts Discussed in Thread: PMP11254 Tool/software: Is it necessary to use the 2512 package for R18 in the PMP11254 design? Due to space constraints, I would like to confirm if a smaller package can be used.
Part Number: TPS23751 Other Parts Discussed in Thread: PMP20220 Tool/software: Hello,
We have designed a PoE power circuit using the TPS23751, and we would like to request a schematic review.
The schematic file is attached: **TPS23751_Schematic_review_250605…
Other Parts Discussed in Thread: TPS23751 , TPS23751EVM-104 Hi Team,
Posting on behalf of our customer.
I'll share this E2E post with our customer so he can reply when needed.
We are currently evaluating a PoE power supply based on the TPS23751…
Part Number: TPS23751 Other Parts Discussed in Thread: PMP11254 , , Tool/software: I would like to replicate the TPS23751 circuitry from the PMP11254 reference design and apply it in a 10G Base network environment. However, since the original reference…
Part Number: TPS23751 Hi Sir,
could you please help review this circuit to see if there any issue? based on our own review, we did not find any problem.
in addition, the MOSFET specification seleected in the attachment appropriate?
thanks for your…
Part Number: TPS23751 Tool/software: Hi,
I want desing PoE PD support 802.3af(15W). But seems 802.3af only can support 12.5W.
I just asked ChatGPT for below modify to meet 802.3af(15W). Is it correct? thanks!
How to design it
Make the device…
Part Number: TPS23751 Tool/software: Hi Sir,
may we know what the problem is?
we found that only the 9v output was abnormal , so we set it to 12v output, after add a load, the output voltage have dropped.
could help us identify or suggestion any…
Part Number: TPS23751 Other Parts Discussed in Thread: TPS26741-Q1 , TPS26744E-Q1 Tool/software: Hi
Could you help me find a complete solution. BUCK+BOOST IC + PD controller, or integration is fine, the architecture is similar to the following.
…