Hi GARETH,
Thanks for your updates.
The layer review sometimes is hard to be accurate and efficient for us since it is hard to know every polygon/trace's net.
Please use the attached layout review instruction and hope it could help for your review…
Part Number: TPS23751 Other Parts Discussed in Thread: TPS23752 Hi team,
My customer ever designed TPS23751 for 802.3at PD(25W) for router application. The sleep mode is MUST have.
And now their end customer is asking higher efficiency PD solution.
So…
Michael Pahl said: Figure 5 and Table 4 give a proposed schematic and part recommendations up to 4kV surge protection. Can you try implementing these components?
In our Board... - SPD1 is applied with a SMCJ58A TVS Diode - SPD2...5 is applied with a Sidactor…
Part Number: TPS23751 I have a PoE SMPS using a TPS23751. I see, that sometimes Type 2 classification is not successful. It depends a lot on the injector. Some do not have a problem at all and some only knowledge the correct tpye-2 classification in 35…
Part Number: TPS23751 my customer has class 4 TPS23751 with RCLS63.4ohms.
if PSE class1(13W) power supply has been attached to this class-4 module, Then Our PoE support power upto13W ? I understand Yes from datasheet sentence but I would like to double…
Part Number: TPS23751 Hello,
Can I Connect the input position of the adapter to the front of the bead and omit the EMI design on the recommended design, as shown on the right
Part Number: TPS23751 Dear Specialists,
My customer is evaluating TPS23751 and has a question.
I would be grateful if you could advise.
---
Regarding CSS of Figure 36 of the datasheet P.37 8.2.2.14,
Could you please let us know the maximum value of Css…
Part Number: TPS23751 Other Parts Discussed in Thread: PMP20220 , HI
We plan to use TPS23751 for POE power supply design. Our design needs to meet 12W output, meet the protection requirements of common mode 6KV and differential mode 2KV. Our design refers…
Part Number: TPS23751 Other Parts Discussed in Thread: PMP20859 , TPS23731 Hi team,
I know we have reference designs with two PD solutions for dual inputs redundant application but wondering if somehow it's feasible to use just one PD or what are the concerns…
Part Number: TPS23751 Hi,
My customer is evaluting TPS23751. but need to change the transformer from refered Wruth 749022011 to EFD15 5V2.7A. they'd like to know if there are some guidance on transformer selection?
does TI have a excel like tools…