Hi Rob,
Thanks for your follow-up.
POE13P-24L looks good for 24-V ~500 mA application. The windings is
If you have a TPS23753AEVM-001, it looks easier to do some jump wires to only configure the secondary side.
If you have a TPS23753AEVM-004, it may…
Part Number: PMP9068 Other Parts Discussed in Thread: PMP11271 , TPS23758 , TPS23753A , TPS23753AEVM-001 , PMP20220 The PMP9068 is setup for 3.3V @ 900mA. Can this circuit be modified for 5V 600mA?
Part Number: TPS23753AEVM-001 Are gerbers or a .brd file available from the factory for TPS23753AEVM-001 evaluation module?
Is there a factory contact?
Thank you.
Part Number: TPS23753A In your evaluation board TPS23753AEVM-001 , there is a BAV99 in the feedback circuit. Can you explain the purpose of this diode? protection?
Part Number: TPS23758 Other Parts Discussed in Thread: TPS2378 , TPS23753AEVM-001 , TPS2378EVM-105 Hi Team,
I have a customer who is interested in using TPS2378 for their project, but they are using RJ45 with magnetic build in. Is there a way to connect…
Part Number: TPS23753AEVM-001 When considering the circuit described in the SLVA433.pdf ( ), if we replace diode D3, flyback diode, from MBRS540T3 to ROHM RB080L-30TE25 (150uA reversed current) or Micro Commercial Components SK53A-L-TP, with a reverse current…
Hi Jens,
Thanks for your information!
Seems your load is about 1 W only (5 V, 100-200 mA). For cost benefit, TPS2372 is used for > 25.5 W (PD Class 5, 6, 7, 8) applications usually considering its passFET's current rating is high.
TPS23758 could…
Hi Chichin,
Sorry that I do not think we have reference circuit with 749119250. While you could look into the following reference designs and make some minor modifications.
PMP7355: 5V, 2A, Class 3,Cost-Optimized,Flyback Converter Reference Design for PoE…
Other Parts Discussed in Thread: TPS23753AEVM-001 , TPS23753A Hi Sirs,
My customer asked the TPS23753AEVM-001 can pass or not pass the 3750VAC (Hi-pot) test?
If they would like to refer the TPS23753AEVM-001 to develop prodcut, the schematics need or not…
Obi,
We don't recommend using diode flyback for 5V output and low power applications as it will give you low efficiency and worse load regulations. You may want to take a look at TPS23753AEVM-001 if you want to design 5V with diode flyback for lower…