Part Number: TPS23755 We are in need of PoE interface with a higher than normal isolation barrier (3kv+). I've reached out to wurth and coilcraft for custom transformers based on the LTD0950 that is recommended for use with the TPS23755. It was mentioned…
Part Number: TPS23755 Hello, I'm evaluating an application where i would need a relatively large voltage span (-15V to +24V) from isolated Power over Ethernet. I was looking at TPS23755 for this role. Due to space constraints, I cannot use the suggested…
Part Number: TPS23755 Hi Team,
We are currently designing an 802.3at PoE PD for one of our PoE products using the TPS23755 controller. During the design process, we found that the recommended transformer parts LDT0950-50 and 750317728 are currently…
Part Number: TPS23755 Hi Team,
We would like to inquire whether you have a solution for a PoE power allocation issue.
Our product is powered by PoE. Inside the system, there is an IP camera powered through PoE, and an AD board driving a 10-inch…
Part Number: TPS23755 Hi,
We found TPS23755 damaged and based on our current measurements:
PoE_GND and PoE_56V- are nearly shorted, with a measured resistance of approximately 12.5ohm
PoE_56V+ and PoE_GND are nearly shorted, with a measured…
Part Number: TPS23755 Hello,
I designed a 12V Flyback power supply able to provide a current of 0.3A using the TPS23755 reference. I used a transformer with the following specifications : - Inductance of 155µH ± 10% - Maximum leakage inductance of 3…
Part Number: TPS23755 Hi Sir,
after reviewing the schematic, we did not find any obvious issue, the design looks good,
could you please review it once more? if have any suggestion or recommend for improvement, we would greatly your feedback and rhe…
Part Number: TPS23755 Other Parts Discussed in Thread: TIDA-010034 Tool/software: The ANCHOR pins (pins A1-A4) are left unconnected in the reference circuit in the datasheet, but on the TIDA-010034 they are connected to VDD, VSS, DAIN, and RSNS. Why are…
Part Number: TPS23755 Other Parts Discussed in Thread: TPS23753A Tool/software: Hi TIer
Do we have POW power which is about 13Watt , Requires secondary output 5V/1.5A, optocoupled feedback, over voltage protection. Do you have more design references…
Part Number: TPS23755 Other Parts Discussed in Thread: BQ25792 , , TPS23758 , TPS23753A Tool/software: Hi,
Can you please check this design for me? We are testing the units now and finding that there is significant ripple on the output and feedback…