Part Number: TPS2378 Tool/software: Hi Michael Pahl ,
we are planning to design a PoE device that is able to get powered over PoE and should be able to forward the remaining power to other daisy chained devices. It seems that I would need the both PD…
Part Number: TPS2378 Other Parts Discussed in Thread: TPS23755 Hi Teams,
Please recommend a POE isolation solution with a smaller PCB footprint, using TPS2378 for POE.
Thank you!
Part Number: TPS2378 Tool/software:
The rough schematic diagram is shown in the figure: The simple principle is that the power from the POE and the power from the DC end are merged through an ideal diode to supply power to a DCDC buck converter for…
Part Number: TPS2378 Tool/software: Hi,
I working on a ethernet application that has a variable power composition from 7W to 15W. On the TPS2378 datasheet I can see the class resistors on table 1. This table mention a minimum power at PD. Does this…
Part Number: TPS2378 Hi TI Engineers Hope this issue finds you well. When I use the TPS2378 to design an IEEE802.3at PD device, I found that when I connect the PowerPad to RTN, the overall power consumption is nearly 1W higher than when the PowerPad is…
Part Number: TPS2378 Other Parts Discussed in Thread: PMP11257 , Tool/software: Hello TI Forum Team,
I have created a schematic of TPS2378PD controller.
I have also implemented the soft start logic for PD controller and 48V to 24V regulator shutdown…
Part Number: TPS2378 Hi Experts,
We are using a TPS2378 as POE powered device to power the product via power-over-ethernet.
At the same moment we are using the option to power the product via a DC voltage, supplied from a DC POWER Jack connector.…
Part Number: TPS2378 Hi TI team,
Per customer-Logitech's request, we need to provide the missing data in the blank columns in below.
Please help fill this out as soon as possible. Much appreciated.
Component PN
Maker Name
Maker…
Part Number: TPS2378 Tool/software:
现用Ti的TPS2378做交换机的 PD接口芯片,按下面原理图做成PD设备。接PSE设备后,无法给该PD设备供电(PSE设备是好的,可以给摄像机供电),量得PD接口处电压在DC3V左右。请分析下原理图有啥问题!
We are currently using Ti's TPS2378 as the PD interface chip and making the PD device according to the following…