Part Number: TPS2379
Hi Team,
Posting on behalf of our customer.
I’ll share this post with our customer so he can reply when needed.
I am trying to design a PoE PD. I am basing my design of the TPS2379DDAR example schematic in the datasheet. Is…
Part Number: TPS2379 Other Parts Discussed in Thread: LM5013 We are using TPS2379 (Non isolated) Please validate the attached Schematic and provide feedback and highlight if any changes required and same we are using LM5013 and LMR51430XFDDCR
Part Number: TPS2379 Other Parts Discussed in Thread: UCC2897A Tool/software: IP Speaker 6Sep2024.rar
We have implemented PoE along with DC mains to operate our board. Requesting to review the PoE section in the layout and please share us your feedback…
Part Number: TPS2379 Other Parts Discussed in Thread: TPS2378EVM-105 Tool/software: I designed and MFR'ed the circuit below and for some reason it's not powering on. At one point a version of the circuit powered on and ran on this POE+ Switch . When I…
Part Number: TPS2379 Other Parts Discussed in Thread: TPS2373 Hi
Test according to the following circuit diagram, the probe is connected before the rectifier bridge. The load is two parallel 194ohm non-inductive resistors, the load power is about 30W…
Part Number: TPS2379 Other Parts Discussed in Thread: TPS23756 , TPS23730 Now WE are looking for a POE chip to replace Si3402B.
PD design requirements are as follows:
1. As a standard IEEE PD, power consumption <5W, 48V and 24V are required, and it…
Part Number: TPS2379 Hi Team,
May I know if TPS2379 support LLDP layer-2 power negotiation ? and how to do the power negotiation?
Thanks & Regards
Eddie
Part Number: TPS2378 Other Parts Discussed in Thread: TPS2379 , Team,
my customer would like to replace TPS2378 with TPS2379.
In their application they are using TPS2378 (APD shorted with RTN – not used internal pass MOSFET).
Looking at the difference…
Part Number: TPS2379 Other Parts Discussed in Thread: UCC2897A Dear all
Please help check TPS2379+UCC2897A SCH and the below issue, thank you!
Attach C30, Generating common ground interference. but no attach C30, ESD very sensitive, 1KV ESD can not…
Other Parts Discussed in Thread: LM2594 Good morning to everyone,
If any of you did, i need to know if it is a good idea to derive 12volt from the POE power supply via the TPS2309 and LM2594HVM-12.
For both I am using the reference drawings.
I have already…