Part Number: TPS2379 Hi Team,
May I know if TPS2379 support LLDP layer-2 power negotiation ? and how to do the power negotiation?
Thanks & Regards
Eddie
Part Number: TPS2379 Other Parts Discussed in Thread: UCC2897A Dear all
Please help check TPS2379+UCC2897A SCH and the below issue, thank you!
Attach C30, Generating common ground interference. but no attach C30, ESD very sensitive, 1KV ESD can not pass…
Part Number: TPS2379 Other Parts Discussed in Thread: TPS23752 , TPS2378 Hi Sir
i can't find replace MAX5981B part.
May TPS2379 can replace MAX5981B?
Bogey
Part Number: TPS2379 Other Parts Discussed in Thread: TPS23861
Hello Experts, I want know recommended PSE device with TPS2379. Would you suggest it? - POE port: 1 - 30W Best Regards, Fujiwara
Part Number: TPS2379 Hi All,
I have tried to measure the voltage on the C bulk capacitor with an oscilloscope to see the voltage raising. When the oscilloscope prove is connected to the C bulk it doesn't do the handshake and I don't know why it is happen…
Part Number: TPS2379 Other Parts Discussed in Thread: TPS23754
We have a customer with our POE PD device which has a TPS2379 IC, they are having the following issue. In all the below situations they are using the Cisco PSE.
Communicating to our device…
Part Number: TPS2379 Hi! TPS2379 datasheet has link on http://www.ti.com/lit/pdf/SLVA498
12.1.1 Related Documentation For related documentation see the following: • Implementing a 60-W, End-to-End PoE System, SLVA498
But this document is not present…
Part Number: TPS2379 The data sheet in Table 1 gives the classification resistor possibilities as 63.4 Ohms, 90.9 Ohms, !37 Ohms, 243 Ohms or 1270 Ohms. The EVM datasheet says in section 3 that a shunt on J7 can be added to give 45.2 Ohms. But that is…