Part Number: TPS2379 Other Parts Discussed in Thread: TPS2378 Hi Expert,
May I know the difference to implement TPS2378 and TPS2379 for high power PD >50W. There are 2 app notes for this topics.
slva498 use single TPS2379 to do this.(SW?)
slva625a…
Part Number: TPS2379 Other Parts Discussed in Thread: PMP7499 Hi Sir, I have question about PMP7499 TI Design and schematic note "If a current sharing PSE is not used, current sharing will be dependent on cable, connector and POE transformer impedances…
Part Number: TPS2372 Other Parts Discussed in Thread: TPS2379 , PMP7499 We are trying to implement a Non-standard 120W Class 8 Powered device. Is there a reference design or some design resource other than the Video shared below.
TPS2372/3 working with…
Part Number: TPS2379 Other Parts Discussed in Thread: TPS23841 , TPS23754 , TPS23861
Does TPS2379(PD) and TPS23841(PSE) can support non-standard POE as block diagram in attached file ? If cannot, which TI can support ? Thank you.
Part Number: TPS2379 Other Parts Discussed in Thread: TPS2373-4EVM-758 Dear Specialists,
My customer'd like to know whether or not TPS2379 is able to use IEEE802.3bt PoE++.
Could you please see the question below and advise?
--- Question
We currently…
Part Number: TPS2379 Dear Specialists,
My customer is confirming TPS2379 circuit.
And he has questions about the result.
Could you please advise?
---questions from the customer---
I have confirmed the operation of IEEE 802.3af PoE (15.4 W) and IEEE 802…
Other Parts Discussed in Thread: TPS2379
Hi
currently i am using TPS2379 for my POE+/UPOE based lighting control appplications . if i have connected more than 15w load to my controller which is based on
TPS2379, the PSE switch is reseting . I request…
Other Parts Discussed in Thread: TPS2379 , TPS2378 I am using TPS2379 in a 50W PoE system. I have a 48V adapter input per OPTION 1 in slva306a, before the TPS2379. Also using the CDB function of TPS2379.
I want to add adapter priority like the TPS2378 has…