Part Number: TPS2379EVM-106 Other Parts Discussed in Thread: TPS2379 , TPS23754 , TPS23730 , TPS23756 Hi Team,
I have a small question, can you have me to test it if you have TPS2379EVM-106.
If connect TPS2379EVM-106 with an non-standard PSE which outputs…
Hi Gabriel,
There are some issues with the ground and input cap.
1. VSS and RTN should not be connected in circuit;
2. EP should be connected to VSS;
3. The data ground normally is isolated and not connected to VSS or RTN;
4. Input capacitance needs to…
Other Parts Discussed in Thread: TPS2379EVM-106 , LM3409HV Hi,
I am trying to control 5 W (400mA * 10 V ) LED load using TPS2379EVM-106 through a an LED Driver circuit. But the load which worked fine independently with the driver circuit powered by 30 V…
Other Parts Discussed in Thread: TPS2379EVM-106 , TPS2379 Hi,
I am planning to use PSE POE29U-1AT with TPS2379EVM-106 to test POE (power over Ethernet ) for 30 W application. My cable length is < 10 m. Can I test this using 25 W load, since as per the datasheet…
Other Parts Discussed in Thread: TPS2379 Dear sir,
I am using TPS2379 EVM-106 along with PSE-phihong 580U as PSE.
But while i connected this PD with phihong PSE out port cable the 3 leds are blinks continuously 3time, it should not connected state, not…
Other Parts Discussed in Thread: TPS2379EVM-106 , TPS2379 Hi,
Is TPS2379EVM-106 designed to comply with Cisco UPOE PSE?
Since it is my customer ask for it.
Thanks and Regards
Part Number: TPS2379 Other Parts Discussed in Thread: TPS23861 , Hi,
we are using TPS2379 for 802.3at POE PD or our product along with TPS23861 PSE.
TPS23861 PSE works fine, but we are having an issue with TPS2379.
We based our design on TPS2379EVM-106 but…
Part Number: TPS2379 Hi All,
I have tried to measure the voltage on the C bulk capacitor with an oscilloscope to see the voltage raising. When the oscilloscope prove is connected to the C bulk it doesn't do the handshake and I don't know why it is happen…
Hi Penny,
Thanks for the response.
I am planning to use the PD evaluation board TPS2379EVM-106 with PSE POE-31U-1AT.
The PSE POE-31U-1AT delivers 30W.
Considering the cable losses, the power delivered to the PD TPS2379 will be 25.5W.
Can you please…
Hi Shaun,
This mostly depends on the data rate of your application. For 10/100BASET applications, you do what is shown in the TPS23756 reference design. For 1000BASET applications, you can do some form of the TPS23754EVM-383. For example TPS2379EVM below…