Because of the Thanksgiving holiday in the U.S., TI E2E™ design support forum responses may be delayed from November 25 through December 2. Thank you for your patience.
Hey Support Team, I don't know the exact reason this TPS2384 is used. But the hardware design is finished and prototypes are available. As far as I know, the TPS2384 is marked as "active" so that there was no reason for our hardware department not to use…
Part Number: TPS2384 Other Parts Discussed in Thread: TPS2490 , TIDA-00465 , PMP20588 HI,
I wanted to know if the above circuit will function properly for a single port PoE standalone application?
Also, does it require a TPS2490 hot-swap controller ?
Part Number: TPS2384 Other Parts Discussed in Thread: TPS23861 Hi Expert,
My cusotmer is reaching to us for standard test using TPS2384. Do you have someting to share with us?
Jimmy
Part Number: TPS2384 Other Parts Discussed in Thread: TPS23861 , TPS2376 Hi. I have rather challenging problem regarding PoE.
I have 2 identical devices which use TPS2384 for PSE, and TPS2376D as PD chip. Both devices has 5 Ethernet ports.
If I connect…
Part Number: TPS2384 Other Parts Discussed in Thread: TPS23882 HI
My customer needs 802.bt 15w 8port VIN 12V to 54V, is there anything suitable for the product recommendation? Thank you
Part Number: TPS2384 Other Parts Discussed in Thread: TPS23861 Hi
The integration capacitor of 0.027uF and the resistor of 124K connected to the Pin 55 do not belong to the customer's component library, hence the customer wants to know:
What is the…
Part Number: TPS23881 Other Parts Discussed in Thread: TPS2384 Tool/software: Hi TI team
Our project use the TPS23881 as PSE controller. For the FUSE, We find two similar case about usage of TPS2384 but we still has some question as below:
1. I saw tha…
Part Number: TPS2384 Hi.
We are developing switches with PoE capabilities.
We implemented PoE protection scheme from TI SLVA233A application note.
Below you can see images of schematics regarding protection and bob smith termination, and PCB.
Problem…
Part Number: TPS2384 Other Parts Discussed in Thread: TPS23861 Hi.
In TPS2384 datasheet it is written that:
Compliant to IEEE 802.3af Standard
Over current threshold is 400mA max.
Meanwhile it can classify PoE Class 4 devices which can use up to 30 W…
Part Number: TPS2384 Other Parts Discussed in Thread: TPS23861 , TPS23882 , TPS23881EVM-008 , TPS23881 Hi TI Team,
We are using TPS2384 quad PSE for a POE application project containing 4 Ethernet ports.In the datasheet of TPS2384 ( http://www.ti.com/lit…