Because of the Thanksgiving holiday in the U.S., TI E2E™ design support forum responses may be delayed from November 25 through December 2. Thank you for your patience.
Part Number: TPS23841 Hello,
I have general some questions regarding the design of POE injectors. I already understand that we need to use a PSE controller such as TPS23841. However, I have other questions regarding the overall circuits and the needs of…
Part Number: TPS23841 Hello,
I have a question about the TPS23841 datasheet. On page 6 it says the threshold for WD_DIS is 1.5 volts, but on page 9 it says ‘connected to 3.3V’.
Does it need to be 3.3 V or could I drive to 1.8 V from our CPU…
Part Number: TPS23841
Hi Team,
Good day.
A we received a query from customer asking if they don't support the AC disconnect feature of TPS23841, what will happen to the device/function?
https://www.ti.com/lit/ds/symlink/tps23841.pdf #page=2
Thank…
Part Number: TPS23841 Hi all,
I have an obsolescence problem with the optocouplers suggested for the I2C communication of TPS23841. Texas Instrument indicates the PS8821-2 in this AN:
http://www.ti.com/lit/an/slva229/slva229.pdf Now these optocouplers are…
Greetings Nakai-San.
The TPS23841 is, indeed, our only Wide Vin PSE. However, we do not offer software support for this PSE as it is an older generation device.
May I ask what end equipment is requiring the Wide Vin?
Thank you for your local support…
Part Number: TPS23841 Other Parts Discussed in Thread: TPS23861 , TPS2388 , TPS23880 Hi,
We've recently developed a couple of prototypes of a PCB that uses the TPS23841 and have just been writing software to interface with the device.
I came across…
Part Number: TPS23841 Other Parts Discussed in Thread: TPS2384 , , EV2400 Hi,
I would like to operate an WiFi access point with POE. Input voltage range of with theWiFi access point: 10 to 30 volts.
For example there is the TPS2384. It can be operated with…
Part Number: TPS23841 Other Parts Discussed in Thread: TPS23861 , TPS2384 Hi,
The customer is evaluating TPS23841.
There is a note on the datasheet Table7 (highlighted with yellow bar below) which is about port enable/disable registers. It has been observed…
Part Number: TPS23841 Other Parts Discussed in Thread: TPS23861 , TPS2388 , Dear Specialists,
My customer is considering POE system and has a question.
I would be grateful if you could advise.
---
POE(IEEE802.3 at) has a two types of alternative mode, A…