Part Number: TPS23861EVM-612 Other Parts Discussed in Thread: TPS2378 , TPS2378EVM-602 , TPS2378EVM-105 , TPS23861 I have connected the TPS2378EVM to a TPS23861EVM-612.
If i use one of the 2 Pair ports the PI-Commander PoE reports immediately that its a…
Part Number: TPS23861EVM-612 Good evening,
Would it be possible to post the schematics, and possibly the footprints used, for the TPS23861EVM-612 evaluation board? I'm looking to use the TPS23861 in an upcoming design, and this would save me quite a bit…
Part Number: TPS23861EVM-612 Other Parts Discussed in Thread: TPS23861 Hi TI support,
We happen to measure surface temperature of TPS23861 in TPS23861EVM-612 & found temperature rise of approx 28-30'C. As such temperature of both operational & non-operational…
Part Number: TPS23861EVM-612 Hi Support,
Would like to ask for the EMC performance/complaince information on the PSU POE module TPS23861EVM-612.
As this module is part of the system test for industrial project.
Thanks.
Part Number: TPS23861EVM-612 Other Parts Discussed in Thread: TPS23861 Good evening,
Would it be possible to post the schematics, and possibly the footprints used, for the TPS23861EVM-612 evaluation board? I'm looking to use the TPS23861 in an upcoming…
Part Number: TPS23861EVM-612 Other Parts Discussed in Thread: TPS23861 There are two kinds of PSE board TPS23861 and the other brand BCM59111, when customer used TPS23861 connect BCM59111 through cable and just supply power for TPS23861, it turns out that…
Part Number: TPS23861EVM-612 Other Parts Discussed in Thread: LM5007 , TPS23861 , LM5017 I'm putting together a PoE injector board using the TS23861 and have seen the eval board.
I was wondering whether somebody could tell me what the expected max output…
Part Number: TPS23861 When operating TPS23861EVM-612 in Auto Mode, why doesn’t the high power port turn on after connecting a standard Type 1 or Type2 PD?
Part Number: TPS23861EVM-612 Other Parts Discussed in Thread: TPS2378 , TPS23861 , TPS2378EVM-105 Hi Sir,
I used TPS23861EVM and TPS2378EVM to test the start up fault. The electrical load is linked to TPS2378 directly with 0.45A to simulate over current…
Other Parts Discussed in Thread: TPS23861EVM-612 , TPS23861 Greetins from Spain.
I have bought a TPS23861EVM-612 and need a switch for 5 ip network (4 POE and 1 no POE)
When i connect devices to TPS23861EVM-612 my pc not connect to network (My pc is one…