Part Number: TPS23861EVM-612 Other Parts Discussed in Thread: TPS23861 Customer is evaluating TPS23861EVM.
If customer use Alternative A connection, Is TPS23861EVM-612's EtherIN connect to the catalog Ether switch no problem?
Or, is it need to use…
Part Number: TPS23754 Other Parts Discussed in Thread: TPS23861 , , TPS23861EVM-612 , TPS23882 Which PSE corresponds to TPS23754? Do we have a whole board solution for PD+PSE cascade?
Other Parts Discussed in Thread: TPS23861EVM-612 , TPS23861 , CSD19537Q3 Hi Sir
May we check if TPS23861EVM-612 can use Si8441AB-D-IS1(1M QUAD-CHANNEL) to replace ISO7241CDW that share existed material in they factory?
Best…
Other Parts Discussed in Thread: TPS23861EVM-612 Hello! I would like use TPS23861EVM-612 for PDs analysis - voltage and current measurement, information about class and things like that. This evaluation board offers everything I could need expect one point…
Hi Paolo,
Let me test and see the behaviors from my end using TPS23861EVM-612 and get back to you tomorrow. Is this issue replicable on all PSEs or only some of them?
Thanks and Regards,
Raymond Lin
Other Parts Discussed in Thread: TPS23861 , TPS23861EVM-612 Hi All,
I am using the TPS23861 EVM kit and trying to test PD as a first step.
I powered the kit and I have USB Interface Adaptor connected to the kit and I am able to see the PI commander GUI…
Hi Hsinwen,
1. Okay I understand the setup now, since both these devices are operating in auto mode, they are both pulsing detection signals and not seeing valid detection. Detection will continue to cycle until valid detection occurs in auto mode. This…
Darwin,
Thank you very much for your comments.
Could you please let me know about TPS23861EVM-612? It has a digital isolation (ISO7241) in I2C line. I guess this system cannot support the clock stretch (or some guy say it as clock low hold) which has one…
Hi Gareth, unfortunately we do not have a block diagram for PCIe with PoE.
For the applications that I have seen for PSEin PCIe schematics, the PSE design is the same as the TPS23861 EVM below. You may consider the schematic in the user's guide to use…