Part Number: TPS23880 Other Parts Discussed in Thread: TPS23881 TPS23881 is the newer generation version of the TPS23880 which has added features and functionality and they are P2P.
and so TPS23881 Spec is better than TPS23880, why we set TPS23880 at higher…
Part Number: TPS23880 Hi Sir,
May I ask one question ?
what is this part mainly used in product ?
no matter poe power or the poe switch , they are already change the project
they are already not use this part right now
what else is…
Part Number: TPS23880 Other Parts Discussed in Thread: TPS23755 , TPS23753A Hi team,
Could you please kindly help recommend a device?
Requirements:
Front connect with Marvell 88e151x PHY
Back connect CAT5e cable
48V DC
Thanks,
Brian
Part Number: TPS23880 Other Parts Discussed in Thread: TPS23881 Hi Expert,
Could you help check the different between TPS23880 and TPS23881? (See as below picture)
Are they P2P and B2B?
I'm not clear the different about reference code and Tumkey firmware…
Part Number: TPS23880 Other Parts Discussed in Thread: TPS23881 Hi Expert,
Could you help check the different between TPS23880 and TPS23881? (See as below picture)
Are they P2P and B2B?
I'm not clear the different about reference code and Tumkey firmware…
Part Number: TPS23880 Other Parts Discussed in Thread: TPS23881 Hi
I'm searching information regarding the difference between the TPS23880 and the TPS23881. We already use the TPS23881. However, because of the chip shortage, we are looking at the…
Part Number: TPS23880 Hi,
in one of our devices we use the TPS23880 poe chip and configured it to provide a maximum power of 60W (Class 6 and not higher). The connected PD is a camera that requires a maximum power
of 50W (inclusive IR and motor) and if…
Part Number: TPS23880 Hi team,
My customer is studying TI PSE solution.
TI separate two tones for single signature and dual signature detection.
May I know what the way to decide which type to start running from PSE? Thanks.
Part Number: TPS23880 Other Parts Discussed in Thread: TPS23882 Hello, Team
may i know if any difference using TPS23880 and TPS23882?
we only need 2 pair, and as i check no different on register map.
Part Number: TPS23880 Hi TI,
I bought a demo TPS23880 kit (mother board + daughter board + MSP430) to test. I download the referent code and run Auto mode. The referent code provides 2 ports 90W and 4 ports 45W. Do you have a referent code that can have…