Part Number: TPS23881B Tool/software: Hi,
I'd like to know if it's possible to use channel 1 for PoE+ Port 1 (802.3at : 2pair 30W) and use channel 2 & 3 for HiPoE Port 2 (802.3bt 4pair 60W) If yes, could you please tell me how to initialize the registers…
Part Number: TPS23881B1EVM-024 Other Parts Discussed in Thread: TPS23881B Please provide link to download latest version of TPS23881B firmware for SRAM and Parity code.
Part Number: TPS23881B Other Parts Discussed in Thread: TPS23881 , Tool/software: Dear E2E Support,
Could you confirm what are the exact differences between our autonomous and former version of TPS23881?
Are we 100% software compatible?
Regards…
Part Number: TPS23881B Tool/software: Hi Dear experts,
I want to use TPS23881B in autonomus mode. I have a question to be sure.
Do I need any micro controller to upload a code to use it in autonomus mode? Or should I just connect AUTO pin (52) to…
Part Number: TPS23861 Other Parts Discussed in Thread: TPS23882B , , TPS23881B , TPS23881
Tool/software:
Hi,
I am trying to choose between the TPS23882B, TPS23881B and TPS23861 PoE controllers. At the moment the project only requires IEEE 802.at…
Part Number: TPS23881B Tool/software: Hi,
I am designing a circuit using the TPS23881B with the following configuration:
3 ports with 2 pairs (2x2)
2 ports with 4 pairs (4x4)
The power supply can provide a maximum of 200W.
Here is the scenario…
Part Number: TPS23881B Other Parts Discussed in Thread: TPS23881 Tool/software: Hi team,
My customer product input signal is POE, it is going through power and data, we want to get the 30W power and 480Mbps data rating, means we need at least the…
Part Number: TPS23881B Tool/software: My issue deals with input: AUTO (Pin#52). I will use this device without MCU. Datasheet mentions: "R_AUTO enables autonomous operation at selectable port power allocation levels." There is no description of these…
Part Number: TPS23881B Other Parts Discussed in Thread: TPS2372 Tool/software: TPS23881B configured as 4 pair 90W, and the 2 pair set power is set as 45W.
If alt-A has a valid signature PD and the PD configured as class 5(45W) but alt-B is open circuit…