Because of the Thanksgiving holiday in the U.S., TI E2E™ design support forum responses may be delayed from November 25 through December 2. Thank you for your patience.
Part Number: TPS2388EVM-612 Other Parts Discussed in Thread: USB2ANY Hi Sir,
The window pop out while connect USB2ANY to TPS2388EVM, what is the next step to do?
Thank you.
Part Number: TPS2388EVM-612 Other Parts Discussed in Thread: USB2ANY Hi Sir,
The user guide of TPS2388EVM mention about USB2ANY adapter, and it's not include in the EVM kit.
How could I get the USB2ANY adapter?
Thank you.
Best Regards,
C.T.Chun…
Hi Cooper,
I2C requires bidirectional channels where each channel should be able to transmit signal both directions. ISO77xx only supports unidirectional channels and hence, it doesn't support I2C as is.
In some applications, the MCU has split SDA…
Hi Randhir,
TPS2384 has over voltage protection at 55V. If you want to test with higher voltage, please use our newer generation PSE EVMs, such as TPS23861EVM-612 or TPS2388EVM. Thanks.
Best regards,
Penny
Hi Vignesh,
Please take a look at TPS2388EVM-612 user's guide and we have a clear flowchart of what needs to be set(the minimum registers you need to set are: 0x12:set operating mode, 0x13:enable DC disconnect, 0x14 enable detection/classification, 0x19…
Hi Brendan,
If the GUI reads the register 0x43 from the PSE device correctly, the device you are talking to is TPS2388, not TPS23880. Can you double check the IC on the EVM is TPS23880 or TPS2388? Is the EVM orderable number TPS23880EVM-008 or TPS2388EVM…
Hello Kapil and thank you for your interest in PoE solutions from Texas Instruments.
The TPS2388EVM-612 gerber files can be found in the tool folder for this EVM at www.ti.com/.../tps2388evm-612 . If you scroll 75% down the page, the gerber files are…
Kevin,
All of our certificates for this device can be found at www.ti.com/.../technicaldocuments . We have the UNH-IOL Interoperability report, UNH-IOL Conformance Test report and SIFOs 802.3 Conformance report.
In addition, we have a reference design…
Hello Chen Bogey8.
The TPS2388 PSE has system software reference code available on the internet here --> www.ti.com/.../toolssoftware and details on how to best utilize/modify that reference code are found within the www.ti.com/.../tps2388evm-612 …
Greetings Jonas. First off, thank you for selecting our TPS23861!
To your question, I am pleased to recommend that you look into the following two solutions:
TPS2388: 8-port IEEE 802.3at-compliant solution. The EVM ( www.ti.com/.../tps2388evm-612…