Part Number: TPS2400
Hello,
I'm planning to use the TPS2400 for a buck converter to implement Over Voltage Protection (OVP) on the output side. Could you kindly review the schematic provided below and advise if it is suitable for the following scenarios…
Part Number: TPS2400 Other Parts Discussed in Thread: TPS25947 hi team,
do we have overvoltage protection controller with normal voltage 20V 7A, while OVP point is 23V?
like Onsemi FPF3381 but can support 7A load current, whether FET internal or external…
Part Number: TPS2400 Other Parts Discussed in Thread: TPS54360 , To Whom it May Concern,
We implemented the low-side switch circuit from your SLVA163 application note and are finding that the MOSFET (PMV213N) is being randomly being damaged in the application…
Part Number: TPS2400 Other Parts Discussed in Thread: TPS25942A Hi,
I'm designing a circuit which has following specification.
Input Voltage 5 - 6.2 V
Input Current 5A
Output Voltage 5V
Output Voltage 5A
According to the TPS2400 datasheet…
Part Number: TPS2400 Other Parts Discussed in Thread: LM25069 , TPS24720 Hello, Fujitsu is using 12V/30A(max) DC supply rail. Since loaded devices absolute maximum input voltage is ~15V, they would like to clamp the 12V rail at 14V maximum. And they are…
Part Number: TPS2400 Other Parts Discussed in Thread: TPS25200 , TPS2595 Hi,
Which efuse device can support 1.8V input? Open to external FET controllers as well.
-Kelvin
Part Number: TPS2400 Other Parts Discussed in Thread: TPS2121 , TPS2663 , TPS2660 Hi team,
my customer is seeing failures with a TPS2121 power mux. the issue was identified as a potential surge on the input pin IN2 exceeding 24V (max rating) from hot…
Part Number: TPS2400 Other Parts Discussed in Thread: TPS2400 , LM5069 , CSD19532Q5B , CSD19536KTT , CSD19535KTT
Our equipment is powered from high capacity LiFePO4 batteries which give a 48V supply output.
I have been evaluating a DC-DC switcher…
Part Number: TPS2400 Other Parts Discussed in Thread: TPS2490 , LM5069 , LM5060 , LM5060-Q1 Hello, I am working on a board for automotive (after market) at 12V (nominal).
It will draw around 5-6 A current.
I want to use a protection IC for load dump…
Part Number: TPS2400 Other Parts Discussed in Thread: LM5060-Q1 Customer doesn't find the recommended ambient temp. it's important for customer used.
application: AC drive/VFD
Customer: WW