Part Number: TPS2412 Other Parts Discussed in Thread: TPS2413 Hi Team ,
My customer when he setting the TPS2412 have some issue.
His PS pin supply the 12V and PS2 unconnect anything.
when he in the no load will see the gate pin waveform show abnormal…
Part Number: UCC29002 Other Parts Discussed in Thread: TPS2412 We are using the UCC29002 and TPS2412 in a load share / hot swap application. Looking into the forum this seems to be a common application.
Now I'm wondering how to deal with the LS pin…
Part Number: TPS2412 Other Parts Discussed in Thread: TPS2413 Hi team,
My customer uses two TPS2412 for input ORing application, see datasheet Fig.10.
However, they met a problem that during normal operation, the low-voltage bus MOSFET was half on…
Part Number: TPS2412 Other Parts Discussed in Thread: CSD17570Q5B , TPS2413 Hi TI,
We have two VR for P5VA and P5VB and this design required redundant feature so we add two TPS2412 for oring control without active current sharing circuitry there due…
Hi
When the input of TPS2412 is left floating, there is a leakage path through the the IC from C pin to A pin.
This leakage current can cause the voltage on the input (A pin) to go higher than 0.8V.
Adding a resistor from A pin to GND, based on…
Part Number: TPS2412 Hi
My customer has a question about Oring FET counts estimation. How do I know how many FET can be used on TPS2412? any application note or criteria? Thanks.
Part Number: TPS2412 Other Parts Discussed in Thread: LM5050-2
Hi,
TPS2412x operating voltage range 3V to 16.5V as specified in datasheet - Is there parts the same/similar to TPS2412 but operating voltage range 36V to 75V? or how do I use the TPS2412…
Hello,
I reviewed your schematics an application note and have the following comments.
1. The UCC29002 was designed for load sharing two power supplies operating in parallel.
A. Please refer to figure 2. Current Sharing in Redundant Systems.pdf…
Part Number: TPS2412 Hi team,
is it safe for the customer to use this device if their expected VCC may drop to 2.7V minimum?
what is the minimum rating for VCC to have expected performance?
Thanks, kevin
Part Number: UCC29002 Other Parts Discussed in Thread: TPS2412
Dear All,
it's me again, still struggling with redundant supply solution with TPS2412 & UCC29002.
The target is 12V/20A redundant power rail. From 2*I6A4W020A033V-001-R from TDK. …