Part Number: TPS2413 We are attempting to use the TPS2413 ICs for a UPS circuit. The battery power source is a 12V battery (operates at ~13.6V), and our main power supply source which is 15V.
The TPS2413 at (U4) which is regulating the Battery power…
Other Parts Discussed in Thread: TPS2413 We are OR'ing 4 power supplies together using the TPS2413. I had originally designed the circuit using a 47.5K resistor for the Rset value due to that we wanted our power supplies to be fully on when they were…
For both TPS2413D and TPS2411D, there are VDD UVLO. What are the response time for these VDD UVLOs?
I mean, when the device is getting VDD UVLO, I think, its “GATE” will be turn off. From the VDD UVLO to GATE turned off, what is the response time?
Other Parts Discussed in Thread: TPS2413 , TPS2412 , TPS2410 In using the TPS2413 we noticed that, even when the FET should be off, the gate pin is ramping and causing glitches of current intot he system. See attached screen shot.
For scope clarification…
Other Parts Discussed in Thread: TPS2413 , TPS2412 Hi,
I have a high current ORing application. Where a set of each 3.3V,5V and 12V, PSUs are ORed and fed to backplane ( cPCI, VME etc) . The current on these PSU can range between 10A to 120A on 3.3V…
Part Number: TPS2412 Other Parts Discussed in Thread: TPS2413 Tool/software: Hi,
I have a customer have an Oring system deamand choose the TPS2412, I would like you dicuss to check if there have new oring solution or TPS2412 is fine.
Please add me…
Part Number: LM5050-1 Other Parts Discussed in Thread: TPS2411 , TPS2412 , TPS2413 , TPS2410 Could you please help to suggest products that can replace ISL6146A
Thanks you
Part Number: TPS25762-Q1 Other Parts Discussed in Thread: TPS2412 , TPS2413 , , LM74700-Q1 , TPS25948 Hi TI,
Due to the client's requirements, I have designed a power structure. Could you please help me confirm if my selection parts is feasible? Or…
Part Number: TPS2412 Other Parts Discussed in Thread: TPS2413 Hi Team ,
My customer when he setting the TPS2412 have some issue.
His PS pin supply the 12V and PS2 unconnect anything.
when he in the no load will see the gate pin waveform show abnormal…
Hi Praveen,
Many thanks for your prompt reply!
Just two additional question:
1. From customer's test results, the Rset value is related to gate voltage, could you please give an explanation why is that?
2. What's the bad impact using TPS2412 linear…