Part Number: TPS2419 I have an application where I need to Diode OR two 5Vdc at 27A outputs using external logic level FETS. Presently we use your LM74700 contoller for our 12V and 28V ORing outputs, but now I need a 5V output solution. Since your LM74700…
Part Number: TPS2419 Tool/software: Dear TI
Regarding the TPS2419 circuit, why is 12VCAP outputting about 1.2V when V1 switch is OFF and V2 switch is ON?
We have confirmed that the gate signal of TR515 is 0V.
I suspect that the leakage current…
Part Number: TPS2419 Tool/software: Hello,
I wanted to use TPS2419 as oring for 5v supply, it having two 5v input from different regulator ranges 4A current. Please verify the drawn circuit if it works or not.
Part Number: TPS2419 Tool/software: Dears:
Customer use TPS2419 to do 3.3V oring, they found below circuit has abnormal high temperature issue
1- Vin=3.3V, load=1A, when do 75C high temperature test, board can't start when store over 5 minutes.
…
Part Number: TPS2419 Tool/software: Hi,
We have a application for Two-Supply Diode-OR Current Balancing Controller with Input voltage 12V/Current 30A.
May I know TPS2419 is suitable for this applcation?
If in both 2 power sourcer exist, 2 TPS2419…
Part Number: TPS2419 Tool/software: Document SLVS998B Layout Considerations
7. C (BYP) should be kept immediately adjacent to the TPS2419 with short leads.
Which of the following is recommended as the PCB pattern connection destination for Cbyp? …
Part Number: TPS2419 Tool/software: Hello, I am using TPS2419 for oring of load voltage with having two power rails input and output to overall load approx 60W.
Please verify this design and let me know can I use this part
Part Number: TPS2419
Hi Team,
TPS2419 controls the combination of two 12V power supplies, which are connected to the NMOS of VISHY externally. Rds=0.0005Ω. RSET is set to 150K. When the two power modules are powered on at the same time, the TPS1249…