Part Number: TPS2420 Other Parts Discussed in Thread: TPS25947 I had a testing design, with a supply of 3.3V.
If the DUT (Device Under Test) circuit had shorted.
Normally it will brown the fuse.
Will efuse like TPS2420, help solve from keep changing the…
Part Number: TPS2420 Other Parts Discussed in Thread: TPS2595 Please let us know how much time is from "detecting Vout<Vin-0.5V" to "PG high(off)"
Regards.
Part Number: TPS2420TPS2420 Technical inquiry - Mr. kang(wbstone@comesta.com)
This is the circuit I have. In addition, Vout has CL = 500uF.
This pictures Normal case(After Power on)
An abnormal current fault case has occurred.(After Power on)
…
Part Number: TPS2420 Hi Team, Need your help on this. Our customer is measuring "offset current" in the 1μA to 2.5μA range in IMON. The measurements are done under load and no load conditions. The load conditions were from 1mA through to 1A, and the output…
Part Number: TPS2420 CT desc says 5uA discharges CT after a fault, but block diagram says 1.25uA and TSD equation calculates to a bout 1.2uA. Which is it? Could the retry time be sped up by switching a resistor in parallel with CT? Are there any limits…
Other Parts Discussed in Thread: TINA-TI , LM3880 , TPS2420 Tool/software: TINA-TI or Spice Models
Hi,
Is there a specific way/procedure to request an unencrypted spices for the LM3880 and TPS2420, or any other spices?
Is there any repository for unencrypted…
Part Number: TPS2420 Hi, Could you tell me about Fault timer flag? Please you check the attached waveform. Is there any protection other than IFLT triggering CT? Customers do not know the reasons for CT startup. Please tell me all the protection that triggers…
Part Number: TPS2420 Hi, Could you tell me about CT pin start condition? CT trigger details are not listed in the data sheet. 1.Could you tell me all the conditions to trigger the CT pin And When power limit is detected at startup,Does the CT pin work? 2…