Part Number: TPS24710 Circuit_proposal_070926.pdf
I have been working on the attached design. Current can either flow from the battery to a load, or from a battery-charger into the battery in reverse direction. I need to protect the circuit from the…
Part Number: TPS24710 Other Parts Discussed in Thread: TIGER Hi,
I used the TPS24710 excel design tool (slvc566f.zip, www.ti.com/.../SLVC566) and my cusotmer is using MOSFET with 700A @ 100uS for SOA curve, but the excel tool cannot enter 700A. Is it…
Part Number: TPS24710 Hi expert,
Customer used TPS24710 and see the Vin has fluctuation during power off. It seems to me the load may drop slower than EN drop below UVLO and energy back drive to input.
They tried to add a cap on EN to GND and no…
Hi,
Welcome to e2e!
FLTB low and PGB high indicates that TPS24710 has remained in current limit long enough for the fault timer to expire and the Gate is pulled low.
While in latch mode, the TIMER pin continues to charge and discharge the attached…
Part Number: TPS24710 Hello Guys,
Good day.
If the TPS24710 has current higher than the fast trip but with short duration (for example 5us), will it shutdown the output current?
Thanks to confirm.
Art
Part Number: TPS24710 Hi there,
Would you be able to share the formula used in the TPS24710 Calculator Tool?
Specifically for Step 3 and 4.
Thank you!
Best regards,
Roy Hsu
Part Number: TPS24710 I am having a hard time correlating the formula for on-time with the example in the datasheet and the Excel calculator. The values do not seem to add up. When I use the values in the example, I get 34usec+2310usec-470usec=1.877msec…
Part Number: TPS24710 Hi,
Is it possible to connect a resistor in parallel with Rsense to fine-tune the current limit threshold ? Could you please give me your advice as the folllowing plans(the plan A and B) ? In addition, is my understanding correct…