Hi Toru,
I think the difference is in one case load current is very high during startup so we are seeing failed startup, VOUT not rising. To check maximum load capability load should be applied after VOUT=VIN.
Regards
Kunal Goel
Part Number: TPS24742 Other Parts Discussed in Thread: TPS25983 Tool/software: Hi there, I 'm doing a design of Priority Power MUX with No HS FET in Primary Power Path using TPS24742. I do not need a HS FET in Primary Power Path of my Priority Power …
Part Number: TPS24742 Other Parts Discussed in Thread: CSD16415Q5 Hi team,
My customer use the TPS24742 to realize r edundant power supplies.
Below picture is the setting parameter from customer sides, Ilimt=9A.
Customer used 'TPS2474x Design Calculator_RevB…
Part Number: TPS24742 Hi experts,
My cusotomer want to use TPS24742 to realize below structure.
There is a question about below picture. If Vin1=Vin2=12V, and Iload=6A, is the current flowing through each channel equal? CH1=CH2=3A? Thanks!
BR,
Gord…
Part Number: TPS24742 Hi,
My customer have a 3 battery backup power system want used TPS2474x.
If they have own MCU can monitor battery voltage level, want used GPIO to control the TPS2474x, how to control the ENOR and ENHS?
Ideal behavior as below:
1.Battery…
Part Number: TPS24742 Other Parts Discussed in Thread: CSD16415Q5 , TPS24741 Hi,
I am using the TPS24742 to build a over current protection and over voltage protection. My target voltage is 14V and current is 20A. I follow the instruction on the datasheet…
Part Number: TPS24742 This applies to the TPS2474x Design-in Calculation Tool Rev B available on the ti.com as of today.
In the Reverse Current Threshold section... (Step 7)
When calculating the min rdson in cell F115, the formula is "F113/F114" This…
Part Number: TPS24742 Hi
Customer wants to know the delay time from OV recovery to the hotswap get driver starts on TPS24742.
Could you give a comment?
Thanks.
Part Number: TPS24742 Other Parts Discussed in Thread: LM25066 Hi,Team,
We can see that TPS24742 has 1.9mS deglich time when recomvey from UVLO conditon.
if IC also has deglich time when recomvery from OV conditon? can we eliminate the deglich time
if…