Part Number: TPS24750 Other Parts Discussed in Thread: TPS24751 , TPS25983 , TPS25990
Hi,
We are considering TPS24750 or TPS24751 as an alternative device for a customer’s 12-V power switch application.
The customer is currently evaluating TPS25983…
Part Number: TPS24750 Other Parts Discussed in Thread: TPS25947 , LM5067
Tool/software:
Hi TI experts,
I need to design the circuit which input signal can be negative voltage and its min value is -5V.
I think if I connect GND pin to -5V, e-fuse…
Part Number: TPS24750 Tool/software: Hello,
I would like to know what the maximum current the load switch can switch at 80C ambient. I am specifically using the TPS24750RUVR in my design.
Part Number: TPS24750 Other Parts Discussed in Thread: TPS25982 Hi,
I want to connect the component TPS24750 to a load who needs 15 amps, this component knows to give a maximum of 12 amps, can I connect two components in parallel?
Part Number: TPS24750 Hello,
I am using TPS24750 on a 8V-1A application. During powering up the input of the Efuse (while keeping Efuse enable pin low) the fault output of the Efuse goes low for 2 microseconds before being released again. This occurs…
Part Number: TPS24750 Hi,
I am using 6 of these power switches in a test fixture. Each one of these TPS24750 is used to enable power, provide current limit in the event of a short and measure the current draw of a unit under test in the fixture (the…
Part Number: TPS24750 Other Parts Discussed in Thread: TPS25982 Hi Team,
Would you advise does TPS24750RUVT have recognition of IEC62368-1 even though
there is a UL 2367 Recognized only in datasheet?
My customer need this information.
Thanks …
Part Number: TPS24750 Hi Team,
Would you advise below three questions about IMON?
(Question) 1. Are you assuming an application in which an AD converter is externally connected to the IMON pin of the TPS24750 to detect the current value of the SENSE…