Part Number: TPS24750 Hi All,
There is the -0.3V absolute maximum limit at the output pin of TPS24750, and in the datasheet there are suggestions to clamp the output with a schottky in case of an inductive load or cable inductance. I suspect that this…
Part Number: TPS24750 Other Parts Discussed in Thread: TPS25982 Hi,
I am designing a circuit with TPS24750 and I would like to simulate my design. However only model available on its webpage is the encrypted PSpice model. Do you have an unencrypted model…
Part Number: TPS24750 Hi,
I am using CSD16570Q5BT as a reverse voltage protection FET. My application is 8V-1A and I need minimal resistance in the E-Fuse+FET. This MOSFET has 10-15nF Ciss. During turn-ON this does not affect my slew rate, but only delays…
Part Number: TPS24750 Other Parts Discussed in Thread: TPS24751 Hi,
On the datasheet it is said that:
GATE is pulled down by a 1-A current source for 13.5 µs when a hard output short circuit occurs and V(VCC – SENSE) is greater than 60 mV, that is, the…
Part Number: TPS24750 Hi,
I am using 6 of these power switches in a test fixture. Each one of these TPS24750 is used to enable power, provide current limit in the event of a short and measure the current draw of a unit under test in the fixture (the test…
Part Number: TPS24750 I have a customer currently evaluating the TPS24750. With a 1.5A load, they are measuring a drain-source drop of 30mV, which suggests a Rds(on) significantly higher than the value listed in the datasheet.
Here's a schematic snippet…
Part Number: TPS24750 Other Parts Discussed in Thread: TPS2662 , TPS2596
Hi Team, My customer wants to limit output current at 100mA when load current increases more than 100mA. He wants not to set fault timer, it is required that 100mA is continue to flow…
Part Number: TPS24750 Other Parts Discussed in Thread: TPS22976
I would like to control a 1.2V rail using the TPS24750. I have a 3.3V bias rail available to power VCC of the IC.
Other than the IMON output being biased essentially from the drain of the…
Part Number: TPS24750 Hi Experts,
We want to know what will happen when Rset resistor opened before power on?
Can it output normally? or what function will be affected?
Thanks.
Part Number: TPS24750 I need to delay the turn on/off operation such that at Vcc rising, turn is is delayed and otherwise turn off is also delayed when Vcc is falling (of course the UVLO is applicable in parallel).
I want to achieve this by connecting…