Other Parts Discussed in Thread: TPS24750 Per IEC 60950 2.5 Limited power sources c), a regulating network, or an integrated circuit (IC) current limiter, limits the output in compliance with Table 2B, both with and without a simulated single fault in…
Part Number: TPS24750 Hi. I'm designing a board using the above-mentioned fuse. I'm wondering if the cap value for the VOUT has to be 470uF. The input voltage is from a low-ripple battery, and will never go above 18V. Can the output cap therefore be lower…
Part Number: TPS24750 Other Parts Discussed in Thread: TPS25982 Hi,
I have design using the TPS24750 as an efuse on a power bus. The design has peripheral devices that can be plugged in after the TPS24750 has already started. These peripheral devices are…
Part Number: TPS24750 Dear Team,
In the TPS24750 reference design. D4 use [Diode, TVS, Uni, 18V, 600W, SMB SMB SMBJ18A-13-F Diodes Inc.]
Can they change to below components?
Please help on making sure these two TVS are suitable or not.
LOSC SMAJ18A DIO…
Part Number: TPS24750 Hi team,
I have some questions about current limit point.
1. Datasheet shows current limit threshold in page 7 is 22.5mV~27.5mV, typical is 25mV. But in page 26, why the threshold is allowed from 10mV~42mV?
2. Is the current flow…
Part Number: TPS24750 Hi, Let's talk about the risk of reverse voltage condition. Customer does not use the "data sheet page 32 Figure 46 circuit" and "clamping/Schottky diode". Customer's circuit image 0243.TPS24750.pdf When the…
Part Number: TPS24750 According to data sheet, the gate capacitor Cgate is calculated by equation 15. An intrinsic capacitor Cintrs is deducted from the first term. In the text above, the value of Cintrs is stated to be about 175pF.
In the design tool…
Part Number: TPS24750 Hi,
I would like to connect the Imon output on the TPS24750 to a ADC input of a microcontroller so that i can monitor the system current consumption. There is not much details on how to do this or specific equations on the datasheet…
Part Number: TPS24750 Other Parts Discussed in Thread: TPS25940 Hi Sir
My customer application TPS24750 in 17V and current limit want set in 5A, but i am not sure which formula can be use? and how to know the accuracy?
…
Part Number: TPS24750 Other Parts Discussed in Thread: TPS25942A Please send details data (i.e. scope plots) of reverse current protection when using the external blocking FET. I don't see anything in the datasheet on this. We would also like to know…