Part Number: TPS2480-81-90-91-92-93_CALC Other Parts Discussed in Thread: TPS2480 , TPS2400 I am in need to do the simulation of the legacy design with TPS2400 part. But I am unable to find the simulation model of the part. Similarly the part TPS2480…
Part Number: TPS2480 Other Parts Discussed in Thread: LM25066 , LM5066 Hello,
The TS2480 datasheet is somehow inconsistent: in the section "Application Information" the name of signals in the text don't correspond to the names on Figures, some typical…
Part Number: TPS2480 Other Parts Discussed in Thread: TPS2490 , TPS2493 , TPS2483 , TPS2482 , TPS2481 , , TPS2491 , TPS2492 , LM5069 , INA293 Dear Madam or Sir,
We are developing a current sense solution involving one of the TI Hot Swap Controllers…
Part Number: TPS2480 Hi,
It is possible to use the TPS2480 at 1kHz with 50% of rcy ?
Because we have a probleme on the rising edge!
Rising edge = 500µs.
What can I check to optimize this timing ?
For information:
-Cout = 1µF
-we have remove…
Hi Rakesh,
Let me make clear about this question.
Below is the data related to TPS2480 read by BMC command in system(Not by TI Tool) .
It seems that controller knows the value of Rshut. And from your last message, the controller 05h register has…
Part Number: TPS2480 Hi dear supporting team,
Would you please help to check TPS2480 “ADC to register store” time and register refresh frequency?
thank you!
Part Number: TPS2480 Hi
There are some layout guide in datasheet, I have two questions:
1. Gate amplifier have hign bandwidth means can accept more noise, so need the trace short, is this right? or some other consideration.
2. The PROG TIMER EN…
Other Parts Discussed in Thread: TPS2480 Hi,
I'm using a TPS2480 to manage power output and I'm having an issue reading data through I2C.
The value I get for the shunt resistor voltage seems to be correct according to my measurements and calculations…
Other Parts Discussed in Thread: TPS2480 I find the data sheet on the TPS2480 very confusing.
I have a External FET that can disipate 3Watts, Its Rds on = 2 mOhms. So if I limit my load current to 15 Amps by using a 3mohm sense resistor. The maximum…