Part Number: TPS2491 Dear Support,
Please advise date code based on the topside marking.
Please refer also to photo. Thanks
1st Line: TI 84
2nd Line: BIX
Part Number: TPS2491 Other Parts Discussed in Thread: TPS1H200A-Q1 , , CSD19537Q3 , TPS2490 , TPS2663 , LM5069 Hi.
I am designing the new industrial data collector of the company, it will also have 2 protected transistor outputs / switches. The nominal system…
Part Number: TPS2491 Per Datasheet the Current Sense Threshold is between 45mV and 55mV with a nominal of 50mV. However on some devices a am experiencing the over-current protection triggers at 40mV. Have these devices got a wider production spread than…
Part Number: TPS2491 Hi,
i got the new PCB . It worked better then the first one. I was able to turn on power bx EN Pin up to a load of 18 Ohms. On higher loads i could not turn on.
After I removed the 330µF Caps on the output the system worked…
Part Number: TPS2491 Other Parts Discussed in Thread: TPS2640 , TPS2662 , TPS2660 I have updated the design calculation for lower load current and soft start. Could you kindly review it?
Estimated MOSFET thermal resistance is on the higher side. Do you recommend…
Part Number: TPS2491 Other Parts Discussed in Thread: TPS2490 ,
Dear e2e team,
My customer would like to replace TPS2491DGS due to delivery issues.
Could you suggest any p2p solutions?
Thanks,
Giorgia
Part Number: TPS2491 Other Parts Discussed in Thread: CSD19536KTT Hi Girls and Guys, I got a problem with my TPS2491 circut. Everything is working fine. But if I hang my 8 ohm resistor as a load between US + and US-, I cannot switch on the system using…
Part Number: TPS2491 Hi Team,
i have some question on tps2491 and hope could get some answers from your side.
1)When used for the electronic circuit breaker function, can the adjustable overload time be repeated 16 times through the fault capacitor? Automatically…