Other Parts Discussed in Thread: TPS2505 , TPS2500 We use TPS2505 Integrated USB power switch. It is not UL listed.
A similar TPS2500 is UL Listed. File No. 169910
Question - is TI planning to TPS2505 UL listed like the TPS2500. If yes, then "when…
Other Parts Discussed in Thread: TPS2500 Hi everybody,
I need some help and I´d really appreciate that.
I want to design an USB OTG device, which could be either host or device.
The used USB transceiver has an enable pin which could used for…
Other Parts Discussed in Thread: BQ24167 , TPS2500 Hi,
I am using BQ24167 dual input charger IC & TPS2500 USB Boost converter in my charger design.
I am able to hear HUM sound from the system.(Mostly near Input section of TPS2500 )
Block Diagram…
Other Parts Discussed in Thread: TPS2500 , TPS2501 Dear All,
In our design TPS2500 boost regulator is operated at light load conditions (Iout <100mA).We are seeing a ripple on Vaux and the switching frequency varies depending on the load current. …
Other Parts Discussed in Thread: TPS2500 , TPS2501 Dear Sir or Madam
I simulated circuit with TPS2500DRCR on test board with no load (see circuit diagram in attached file). My result (see Fig upper left in the attached file) is battery voltage decrease…
Part Number: TPS25200 Other Parts Discussed in Thread: TPS2500 , , TLV62585 Hello Team ,
We are planing to use TPS2500 IC in our board for over voltage and over current protection.
But we need a reverse voltage protection with this IC .
We are planing…
Hello,
You will need to add a dc-dc to boost the voltage from the 3~4.4V or higher for 5V on VBUS or higher if you wish to use Type-C PD.
You could use a device like the TPS2500 that has a built in dc-dc, but from what I know of the part, it is…