Part Number: TPS2511 Tool/software: Dears,
TPS2511 can only support type A, is there any device that supports Type C? Is there any device that can be used with SY9601P2P and supports Type C?
Thanks!
Part Number: TPS2511 Tool/software: Hi TI team,
Please help to provide name and location of fab and assembly & testing for below items with COO. Thanks.
TPS2511DGNR
TPS3813K33-Q1
Part Number: TPS2511 I see the USB port IC datasheet.
That has some difference of RDSon value of two parts.
TPS2511Q1 is 80mR, TPS2511 is 70mR.
Why they are different?
Is that difference line?
If design is difference, please inform me what is…
Hi ,
There are several differences between the HBM and IEC 61000-4-2 standard that are immediately obvious. If you use the IEC standard to test the TPS2511, it will be failed even though you say the test voltage is 5KV , In the same 5KV , IEC may create…
Part Number: TPS2511 Other Parts Discussed in Thread: TPS54240 , Hi there,
For a customer we have developed a system incorporating the TPS2511 and TPS54240 controllers. The board has a micro USB out for dimension reasons. Connecting a phone with an…
Part Number: TPS2511-Q1 Other Parts Discussed in Thread: TPS2549-Q1 Hi, TI Support Team
Inquiries for replacement products for the following products have been received from customers.
TPS2511QDGNRQ1
TPS2511DGNR
If there are alternative products…
yes TPS2511 role is DCP
there isnt any device on the bus line. but iphone 4s charged with apple 30pin to usb cable, Is this a problem?
and i have some question to:
1.is there another circuit to use TPS2511 for charger?
2.is TPS2511 can Detect all…
Part Number: TPS2511 Other Parts Discussed in Thread: TPS2549 , , TPS2546 Hi team,
My customer need a 10W type A that is dedicated for charge. Customer hopes the solution is simple and easy for design. Is the TPS2511 or TPS2549 suitable? Thanks.