Part Number: TPS2514 Other Parts Discussed in Thread: TPS2546 My customer is considering using our TPS2514 device. But his application only need D+D- only USB DCP applying 1.2V, current 0.9A-1.1A, But our TPS2514 could support D+D- 1.2V, and also D+ 2…
Other Parts Discussed in Thread: TPS2514 , TPS2514A Hi team,
I have a question about the TPS2514. Can it support Iphone 6S and iphone 6S plus?
My customer uses TPS2514 in usb port but can't charge the iphone7. When they plug in the iphone7, the D+ D- is…
Other Parts Discussed in Thread: TPS2514 Hi,
Do we have a report for the TPS2514,I want to know it supports which phone and Tablet. And how much current per cell phone and Tablet supports when using TPS2514?
Thanks!
Part Number: TPS25810 Other Parts Discussed in Thread: TPS2514 , TPS25814 , TPS25750 Hello.
I am designing with the TPS25810 abd I am doing further tests, using the following equipment:
- TPS25810 Evaluation board
- Commercial charger with 5V/15W output …
Other Parts Discussed in Thread: TPS2514 I am performing a FMEA on the TPS2514 and I am wondering what are the effects of the circuit or users PED when then DP or DM pins:
1. Short to Ground
2. Fail Open.
Also, do the next failure modes make sense, and if…
Other Parts Discussed in Thread: TPS2514 , STRIKE I am wondering what are the failure effects if there was an issue with the pins for the TPS2514 Dedicated USB Controller. More specifically what happens with DP1 and DM1 when there is an issue. The issues…
Other Parts Discussed in Thread: TPS2514 , TPS2541 , TPS2511 Hello,
In one of the project I am using BQ24055 for charging the internal battery of the device. In the same project I have a AC-DC converter of 3V (5V,600mAh). I want to use the AC-DC converter…
Part Number: TPS25810 Other Parts Discussed in Thread: TPS2514 , TPS2546 Hi team,
We have seen that TPS25810 is used with BC1.2 in datasheet.
Can this application be used with TPS2546 instead of TPS2514?
In addition, when there're both VCONN's power (5V3A…
Dear Adam,
Thanks for the comments. We appreciated your great support!
Our customer believe your proposal of TPS25810 with TPS2514 is a good solution on standard USB C-type charger.
They want to ask you , could TPS2513A with TPS2561A solution support…