Part Number: TPS25200 Other Parts Discussed in Thread: TPS2553 , Hi,
I'm working on a design which involves migration from a TPS2553 power switch onto TPS25200 eFuse design since I'm allocation same board space for the DRVR package & there's additional…
Part Number: TPS25200 Hi Sir,
Below is TPS25200 output voltage clamping SPEC.Its max voltage is 5.55V.
We have below 3 requirement.Thank you.
Could you provide the quantity percentage of output voltage clamping is 5.5~5.55V?
And is there any pin to pin…
Part Number: TPS25200 I have used TPS25200 for the purpose of the current limitation in my circuit. I have used 60.4Kohm for Rlim, and using equation 1 of the datasheet, Ios nominal will be approximately 1.5A. For testing, I used the potentiometer to…
Part Number: TPS25200 Hi, Good day. I hope everything is fine. Our customer has a question regarding the thermal information for TPS25200. In the datasheet the parameter Rja (chapter 6.4) is 66.5°C/W. To obtain this value which footprint was used? (for exposed…
Hi Devipriya,
In eFuse, auto qualified we only have TPS25940-Q1, TPS25200-Q1.
Hotswap have timer pin which you can set to allow current transient. After timer only device will shut off.
Robust Hot Swap Design (Rev. A) (ti.com)
You can also check ideal…
Part Number: TPS25200 Hi,
According to TPS25200 datasheet, Capacitor is connected between Vin pin line and GND. I think this capacitor is added for stable voltage input on Vin pin. Is it correct? Please let me know.
If clean voltage is supplied from…
Part Number: TPS25200 I'd like to use this device for current limiting on the SD Card power circuit.
Could you please tell me which should I use equation 1 or Figure17,18 in datasheet(SLVSCJ0C) page.15?
I think that both results don't match.
…
Part Number: TPS25200 Hello expert, I have request to you regarding IEC62368-1. On the TI.com, there is the document TPS25200 UL certification of compliance IEC62368-1 . However the document is certification letter of IEC-60950. So would you provide certification…
Part Number: TPS25200 Hi
I have a question about current limit accuracy of TPS25200. Are Iosmin and Iosmax of equation(1) the value at Tj=-40~125℃?
Best regards,
Yokota
Part Number: TPS25200-Q1 Dear TI team,
is-there an ESD diode between nFAULT pin and VIN for the device TPS25200-Q1?
In our desgin, we would like to apply a voltage on nFAULT pin (3.3V, via a 10k pull-up resistor) when its input voltage is 0V. Will this…