Part Number: TPS2521 Other Parts Discussed in Thread: SN74AHC1G02 , SN74AHC1G32 Hi all,
i have set the UVLO limit on TPS25210ARPW to 4.5V like so:
and i want to drive the EN pin from external NOR SN74AHC1G02 gates ( push-pull output) like
is this ok,…
Part Number: TPS2521 Hello,
My customer is asking me a question for stencil design of TPS2521 that is described on P45 of the datasheet(SLVSFX8).
It says that “BASED on 0.100 mm THICK STENCIL”.
But they usually uses 0.130mm thick stencil…
Part Number: TPS2521 Hi team,
I'd like to order TPS25210EVM for my customer.
Is TPS25210EVM available at TI.com?
I could only find the EVM user guide, but I can't find EVM web page and EVM order link.
Regards,
Itoh
Part Number: TPS2521 Hello Experts, Would you please tell Absolute Maximum Ratings of OUT-pin? The datasheet stated that MAX is "min (28, VIN + 21)". What does it mean? If VIN=28V, ABS of OUT-pin is 28+21=49V? Best Regards, Fujiwara
Part Number: TPS2521 Hi team,
My customer is trying to use TPS25210ARPWR for USB VBUS (5V) output protection (OVP, OCP).
Current limit should be 0.5A (RLIM=6.65kOhm).
About OVP, it is needed to be clamped within <6.5V so OVCSEL pin will be left floating…
Hi Fergus,
THX for your help.
I did some research on eFuses and here is what i came up with:
https://www.ti.com/product/TPS2521?dcmp=dsproject&hqs=#order-quality TPS25947 https://www.ti.com/product/TPS2521
It is only for the cell so i think it is good…
Part Number: LM74700-Q1 Other Parts Discussed in Thread: LM74502-Q1 , , TPS25961 , TPS2521 , TPS25947 , LM74800-Q1 , TPS2663 , LM76202-Q1 Simple question - I'm considering using the LM74700QDBVRQ1 as a NMOS power (DC) switch controller. Can I connect the…