Part Number: TPS2549 I’ve encountered some issues while using the tps2549, and I need assistance in resolving them. We used the DCP mode and tested some smartphones, but none of the currents reached the specified values of 5V and 1.5A mentioned in the…
Part Number: TPS2549 I am using the TPS2549 for USB 2.0 DP/DM handshake. I am not using the power switch functionality. As such, I only need to power the IN pin with 5V.
What do I do with these unused pins? OUT, CS, ILIM_LO, ILIM_HI. Do I need to float…
Part Number: TPS2549 I have a device with a USB peripheral capable of detecting the remote side using the BC 1.2 specification. When the TPS2549 is configured as a SDP or CDP, I am able to correctly identify this. However, when configuring the TPS2549…
Part Number: TPS2549-Q1 Other Parts Discussed in Thread: TPS2549 , We are using the TPS2549‑Q1 in an automotive design.
During ADB connection, an external device (laptop) may supply 5V on the USB VBUS, which appears at the OUT pin of the IC. This creates…
Part Number: TPS2549-Q1 Other Parts Discussed in Thread: TPS54260-Q1 , Hi TI Support Team,
We are currently developing an automotive infotainment project and would like to request your support in reviewing our schematic design.
In our design:
…
Part Number: TPS2549-Q1 Hi team,
We need the solution to implement.
USB A type _2 ports
-Support 5V/ Min 3A
- Support Carplay, Android Auto
Please help to suggest.
Thanks,
Leo
Part Number: TPS2549-Q1 Other Parts Discussed in Thread: TPS2549 , Tool/software: Could you please help me for schematic review for customer of TPS2549
Part Number: TPS2549 Tool/software: Hi Sir
We have a question about TPS2549RTE.
When charging a phone via the TPS2549RTE, if the phone is restarted while keeping the USB connection intact, the phone is no longer recognized
(ADB devices fail to…
Part Number: TPS2549-Q1 Hi Team,
I am estimating the power dissipation of the TPS2549IRTERQ1 device for heatsink design.
My understanding is that the dominant IC power dissipation is due to the internal MOSFET conduction loss and can be calculated…
Part Number: TPS2549 Other Parts Discussed in Thread: TPS2546 Tool/software: Hi all,
Does TPS2549/TPS2546 support APPLE 2.4A? Do we have a device that supports Apple 2.4A?
Many thanks!
Arabella Zhang