Part Number: TPS2552 My device need to realize the High-Power Functions application.
High-power functions must draw less than 100 mA at power up and can draw up to 500 mA after enumeration.
How can I realize this current limit requirement by using…
Part Number: TPS2552 Hi,
I am using TPS2552 for 5V supply to external circuitry from my board controlled by enable pin of TPS2552. The OUT pin of TPS2552 is connected to external connector pin. In case if 12V or 24V is applied on this OUT pin because…
Part Number: TPS2552-1 Tool/software: Hi,
We are using this part to provide a 2 level current limit based on a GPIO output.
We would like the lower limit 75mA, and the upper limit close to 1A.
We have tested with the following configuration and…
Part Number: TPS2552 Dear Ti team,
do you have any detailed information about the current limitation accuracy when the TPS255xx is set to output 190mA abs. max.?
Best regards
Part Number: TPS2552 Tool/software: Hello TI,
Currently, I am working on a project that involves connection of USB LTE Cellular Dongle on USB TYPE A connector and it requires 600mA typical for continuous operation. Therefore, I have included TPS2552…
Part Number: TPS2552 Other Parts Discussed in Thread: TPS2553 , , , TPS2553D Tool/software: Hi Team,
Could you help ex[plain why TPS2552 and TPS2553 pricing are different?
As I know just EN active H or L. others are all the same.
Part Number: TPS2552-1 Hi team
Our customer want to know about FAULT de-assert timing with EN control on this device.
When I checked the datasheet p14 9.3.3 FAULT Response , I found the following statement, which says that the FAULT signal is de…
Part Number: TPS2552-1 Other Parts Discussed in Thread: TPS2553-1 , TPS2553-Q1 , TPS2553 , TPS2552 Hello guys,
I have seen that the model TPS2552-1 is very similar to the TPS2553-1 (only enable pin is different) but there is no automotive version…