Part Number: TPS2553-Q1 Other Parts Discussed in Thread: TPS2553 , Hello,
We succesfully use comemrcial version of switch - TPS2553. Measured Rdson "(U_IN - U_OUT)/I_OUT" is fine. Transition to current limit mode is fine - linear and stable. R_ILIM…
Part Number: TPS2553-1 Hello,
I would like to know if Texas Instruments provides any MTBF or FIT data for the device TPS2553DBVR-1.
The device is used under continuous operation at an ambient temperature of 70 °C.
If no part-specific MTBF…
Part Number: TPS2553 Hi Team,
Interested in using the TPS2553's auto-retry capabilities mentioned in the datasheet.
I know the part doesn't have any hysteresis on the EN pin, so I'm looking for specifications on a MIN time ~FAULT is pulled low during…
Part Number: TPS2553 Other Parts Discussed in Thread: TPS2001D , Hi Team
My customer side meet a issue as below.
they insert a USB2 cable with power(5V). they find if system shut down. Vout/Vin can't close normally.
We have tried TPS2001D…
Part Number: TPS2553 Tool/software: Dear tem,
Good day!
Here i bought TPS2553DBVR twice from Mouser, but our QC team found X-ray results showed bonding wires and lead frame are different between 2022DC and 2024DC, could you help advise if ther are…
Part Number: TPS2553 Tool/software: Hi team:
we have a question when we use the part TPS2553, especially for the input and output capacitance value for choose.
our schematic diagram as follows:
background:
the load the output of TPS2553 is 60mA…
Part Number: TPS2553-Q1 Tool/software: From the functional safety information TPS2553-Q1 Functional Safety, FIT Rate, Failure Mode Distribution and Pin FMA .
I'm a bit confused from this document. Is 3 Failure Mode Distribution (FMD) applicable to Table…
Part Number: TPS2553 Hi Team,
Customer want to confirm if TPS2553 can be used as hotswap/efuse? The output is USB interface and the input will also be hotplug. Is it ok for this use case if they place TVS at the input side of TPS2553 and place Schottky…