Part Number: TPS2549 Other Parts Discussed in Thread: TPS2556-Q1 , In your application report named "How to Pass MFi Overcurrent Protection Test With USB Charger and Switch Device", It has mentioned that MFI OCP test can be passed with TPS254…
Hi Kinjoh-san,
The output voltage depends on the impedance of the short. If it is a hot-short at the output, the output voltage falls close to zero.
The device can maintain VOUT to an certain extent for overload condition.
Thanks
Rakesh
Other Parts Discussed in Thread: TPS2556 , TPS2552 Dear Sir
Good days,
The TPS2556 suggest Rilim rang is 20K~187K, but when we set up output current limit is 0.5A.
the calculate Rilim is about 220Kohm. May we check with you if Rilim over 187Kohm, is there…
Other Parts Discussed in Thread: TPS2556 , TPS2553 , TPS2561 , TPS2560 , TPS2552 Dear TI
Customer has a question of TPS2556/2557 in Figure20 on datasheet page14.
1kohm resistor is connected to fault pin in series with 100kohm.
But similar devices which TPS2553…
Other Parts Discussed in Thread: TPS2556 , TPS2557 Dear All,
can yo recommend a load switch that covers Type C 5V 3A with EN and FLT pin?
Like NX5P3363
Best Regards,
David.
Other Parts Discussed in Thread: TPS2556 Dear Sir
May we check if TPS2556 output side need add 150uF capacitor? or we can direct connect to Load side? Best regards Bogey
Other Parts Discussed in Thread: TPS2556 Hi folks,
I was checking TPS2556/7, this may be very naive question, but I am curous to know about the purpose of two inputs in tps2556/7. Does this package contains two independent blocks? Maximum total input voltage…
Part Number: TPS2042B Other Parts Discussed in Thread: TPS2556 , TPS2066 , TPS2064 , TPS2560 , TPS2052 , TPS2557 Hi Team,
a customer asks if there is a suitable alternative for the TPS2042BDR. (preferably p2p)
Thanks and regards
Roman
Hi Zirui,
Don't have p2p device. But have similar function device, such as TPS2556-Q1 and TPS2557-Q1.
For TI's policy, I will first click resolved button.
If you have any other concern, contact me any time.
If you think resolved, please help…