Part Number: TPS2561 Other Parts Discussed in Thread: TPS25980 , TPS25946 Tool/software: I'm wondering if the Efuse TPS2561 can block the reverse current from out to in. The blocking MOS or diode seems not implemented based on the datasheet. What about…
Part Number: TPS2561 Tool/software: Hi,
When the TPS2561 EN pin is disabled, is it possible for current to flow back from +5V2 to the input terminal (+5V1)?
If the answer is yes, I will consider adding a diode to the input side to prevent backflow.
…
Part Number: TPS2561 Hi Experts, Good day. Please help provide the Input voltage rise time of TPS2561. In the datasheet, the only available info is the output rise time. Regards, Josel
Part Number: TPS2561 Hi Sir,
I tested TPS2561 with different current limit setting and got abnormal behavior when over current occur.
For 1.4A current limit, TPS2561 is auto retry when OC occur; but for 1A current limit setting, TPS2561 isn't auto retry…
Part Number: TPS2561 I design set-top box have USB port
TPS2561 is designed for USB, and for IEC62386-1 certification.( US-37138-UL)
But TPS2561 doesn't have Input Over Voltage LockOut(or Clamping).
How certificate IEC62386-1 with TPS2561?
Is TPS2561…
Part Number: TPS2561 Hi TI Expert,
For below auto-retry implementation, when OC happens, the fault is pulled low and 0.22uF cap will be discharged through FAULT pins.
Is there any pull-down resistance to limit the discharge current?
Thanks
Part Number: TPS2561 Other Parts Discussed in Thread: TPS2560 Hello Expert,
I have a question.
Is there internal Pull-up or Pull-down resistor in EN pin which is TPS2561, TPS2560?
If yes, what's the resistor value?
Best regards,
Michael