Part Number: TPS25730 Other Parts Discussed in Thread: TPS25751 , TPS65987 Is it possible to use TPS25730 in combination with TUSB1046 to control the power delivery on usb c port with power delivery (as a sink) and usb 3 and DP alt mode capabilities.…
Part Number: TPS25730 Hello,
The October 2023 Initial Release datasheet for TPS25730D VBUS pin claims the I/O type as O (Output) in Table 5-1. I assume this should actually be I (Input)?
Thank you,
-- Matt
Part Number: TPS25730 Other Parts Discussed in Thread: TPS25751
Hi Team,
Posting on behalf of our customer.
We are currently evaluating to use the TPS25730D in a design.
I would like to be able to use the ADC inputs for other analog measurements…
Part Number: TPS25730 Tool/software: Hi,
Since there is already an FET on the power path controller, I would like to operate the TPS25730S without an FET.
Is this possible?
How must VSYS be connected, directly to VBUS?
What else needs to be…
Part Number: TPS25730 Hi Team,
Please assist with schematic review.
Can the LDO_3V3 be connected to VIN_3V3 to supply power to VIN_3V3?
Or an additional 3V3 power supply is required to VIN_3V3.
Part Number: TPS25730 Hi Team, I got a question from customer, could you please kindly help to clarify it?
They are confused that why the application design needs a dual channel FET?
Could you help to clarify if it is mandatory or we can just use…
Part Number: TPS25730 Tool/software: After a couple prototype revisions of TPS25730 and several reads of the datasheet, my prototypes still produced no output. I've been a EE for 18 years--this should have been a cakewalk.
Convinced of a datasheet omission…
Part Number: TPS25730 Other Parts Discussed in Thread: TPS25751 Hello,
I am using the TPS25730 in sink mode and would like to dynamically change voltage/current requirements at runtime via I2C , similar to what is possible with TPS25751.
Application…
Part Number: TPS25730 Other Parts Discussed in Thread: TPS25751 Hi Team,
The TPS25730 is normally in sink mode, receiving 15V/3A power.
When the system is powered by other means...
Can the TPS25730 connect to a USB 2.0 flash drive for data transfer…
Part Number: TPS25730 Hi, Please review the attached schematics using TI PD charger IC (P/N - TPS25730D). Suggest any comments if to be implemented. Thank you.
Power.pdf