Part Number: TPS25730EVM Other Parts Discussed in Thread: TPS25730 Hello team,
My customer is reviewing TPS25730 with EVM, but there is a problem in the user guide.
The customer got EVM Rev.A2, but some contents are not modified from Rev.A1. Can you please…
Part Number: TPS25730 Tool/software: The datasheet for TPS25730D denotes pin 36 as RESERVED. However, in the TPS25730EVM user's guide, pin 36 is labelled as FAULT_OUT. Which is it?
Hi Gaurav,
The only external components required for the TPS25730 are resistors and capacitors, which are also needed for the CH224K. If you look at the TPS25730EVM, the solution size is highlighted in the white box. Reinforcing that only passive components…
Part Number: TPS25730 Tool/software: We're working with the tps25730d. The datasheet indicates pins 26, 27, 36 should be tied to either ground or the LDO. But when working with the evaluation module and looking into the users guide we notice that…
Hi Jacob,
Apologies are the confusion, table 8-1 can also be applied for ACIN3 and ADCIN4 as well. There are no differences between the DIV calculation for all of the ADCINx pins.
You can refer to the TPS25730EVM as a reference, all the resistor divider…
Hi Aya
I just received USB-PD-CHG-EVM-01 evaluation board from TI. If I connect this board to the TPS25730EVM sink board, I get the same problem namely the TPS25730EVM being turned on and off due to missing 9V on VBUS. However this happens if I supply t…
Part Number: TPS25730 Other Parts Discussed in Thread: , TPS25751 Hello,
I just received the TPS25730EVM and I am trying some configurations. I have a USB-C Dell Laptop PS that outputs 5V and 20V only.
Run
Min Voltage
Max Voltage
PPHV Output
Commen…
Barrel Connectors Compared to USB-C®
Unlike a majority of barrel connectors, USB-C® is a standardized and regulated interface that is become common place across multiple different industries. The USB-C® connector as well as the USB-C and USB-C Power…